This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Expert,
F280025, Uniflash can not reset device and run after programming hex file, it is ok to reset the device with out file,
but not able to reset and run the code when download hex file, it may be a bug and can be reproduced by Ti c2000ware example,
could you help check if anything wrong?
F280025, Uniflash can not reset device and run after programming hex file, it is ok to reset the device with out file,
After you have programmed with hex file, does the program run after disconnecting then reconnecting the debugger (USB) cable?
can be reproduced by Ti c2000ware example,
Which example please?
could you help check if anything wrong?
Perhaps the debug probe remains connected in which case the program will not run. Try deselecting the following:
Hi Kier,
you can reproduce this issue with below example code with F280025_launchpad, the led is blinking after downloading out file,
but never change after download hex file.
I could not find a difference between your .out file and your .hex file.
I could not replicate the problem with 'launchxl_ex1_f280039c_demo'.
Do you use the same .uniflash session file for both .out and .hex?
There should be ok for F280039, you need to reproduce this issue with F280025
I mean do you use the same session file? So you either select and program Image 1 or Image 2:
I don't have the F280025. I only have the F280039 launchpad. Anyway, I doubt the difference is relevant.
I always use image 1 only, I always use F280039 to do the test, seem also have the same issue,
is anything wrong for the hex generation?
is anything wrong for the hex generation?
No, I don't think so. I checked it is the same contents as your .out file.
Please post your UniFlash session file (.uniflash)
Ah. Now I can replicate your problem. Let me invite TI to comment.....
Hello Ki. Ki
I believe this is another instance of the issue I reported in my post from a few weeks ago but didn't quite get to the bottom of:
Both in the demo project from Strong Zhang (launchxl_ex1_f280025c_demo) and the equivalent example I tried today (launchxl_ex1_f280039c_demo) there is indeed a difference in UniFlash behaviour between a .out and .hex file when all other things are equal.
'Run Target' is successful for .out only but not for .hex. The latter is my use case in my original post above.
I checked with dis2000 that there weren't additional sections present in the .out file that are missing in the .hex file and, in any case, cycling the power of the launchpad after flashing the .hex does indeed run the program. Furthermore there is no difference in the verbose logs of flashing .out and .hex.
So please can you try to replicate the problem and therefore explain why the .hex load image does not 'Run Target'?
'Run Target' is successful for .out only but not for .hex. The latter is my use case in my original post above.
I was trying this out in CCS. When I load the generated *.out file, the PC (Program Counter) is set to 0x80000. From there it will disable the watchdog and then jump to the entry point of the application (_c_int00). Eventually it will run to main and beyond.
When loading the *.hex file, the PC is set to 0x0 and then just gets stuck somewhere. Doing a disconnect, then connect, then disconnect again will cause the program to run as expected. A power cycle will do the same also.
The symbols in the out file will have the program entry point location and other debug symbol information while that is missing from the hex file.
I guess I am unsure if this is expected behavior or not. Perhaps someone from the C2000 team can comment.
Thanks
ki
Reset Action to CPU reset after loa
Many thanks. That workaround works for me.
When loading the *.hex file, the PC is set to 0x0
You finally got to the root cause, thank you very much. This has bugged me for years!
One possible explanation for the difference is that the label 'code_start' flash entry point (0x80000) only exists in the .out file. Having said that, the flash entry point can be assumed 90% of the time to be 0x80000 (in the case of F28003x and others) since it is a characteristic of the silicon:
Perhaps a UniFlash enhancement to type in the Flash Entry Point address in the UniFlash GUI (saved with the session file) next to 'Run target' might make this behaviour transparent and controllable for hex file users? In the case of a .out file, this box could be greyed out and the contents replaced with the 'code_start' address.
Mock-up:
I have been playing around with this a bit today and noticed that if I enable the option to perform a CPU reset after program load, the program will run as expected as long as I disabled the option to remain connected after operations. Maybe this is a viable workaround.