Part Number: TMDSDOCK28069
Other Parts Discussed in Thread: TMDSCNCD28069, C2000WARE
I have the following hardware:
Docking-Stn USB-EMU, [R3] (TMDSDOCK28069) https://www.ti.com/tool/TMDSDOCK28069
and the
controlCARD F28069, Release 1.1 (TMDSCNCD28069) https://www.ti.com/tool/TMDSCNCD28069
I follow the steps to access schematics for these, at C2000Ware location:
boards\ExperimenterKits\DockingStation_DIM_100pin\R3 &
boards\controlCARDs\TMDSCNCD28069\R1_1
However about 15 DIM pins are mislabeled between the DIM on schematic of the controlCARD and that of the Dock.
For example, in the image below, the dock's DIM pin 81 is labeled as "GPIO-85", and also in silk screen as "85".. But there is no GPIO 85 on the F28069!

On Docking station DIM100:

But on controlCARD DIM100:

Bigger list of inconsistencies:
DIM pin # / Net name on controlCARD / Net name on Dock
20 / GPIO54 / GPIO60
22 / GPIO56 / GPIO62
30 / GPIO40 / GPIO48
31 / GPIO42 / GPIO84
32 / GPIO50 / GPIO86
42 / GPIO51 / GPIO87
68 / GPIO44 / GPIO59
70 / GPIO55 / GPIO61
72 / GPIO57 / GPIO63
80 / GPIO41 / GPIO49
81 / GPIO43 / GPIO85
Am I missing something?