Other Parts Discussed in Thread: C2000WARE
Hello,
I am using two launchPads for CAN practice. I use the code from "C:\ti\C2000Ware_4_03_00_00\device_support\f2837xd\examples\cpu1\can_loopback_bitfields\cpu01\can_loopback_bitfields.c" to program it. The LED D1 is solid green, D9 solid red, D10 solid blue. The user's guide says: "If the sample is above mid-scale (2048), the blue LED D10 will illuminate. If the sample is below mid-scale, the red LED D9 will illuminate." So when both LEDs are illuminating, what does it mean? What is wrong with it? Does it show normal operation when D9 is red and D10 is off, otherwise?
Thanks,
Hongmei