Part Number: TMS320F28388D
Hi Expert,
My customer want to do over current protection by using 12 comparators inside F28388, then send 12 different CMPSS event signal to different PWM modules.
what they require is to use all 12 TRIP signal below, there is no issue to use TRIP4, TRIP5,TRIP7,,, which connected to ePWM X-BAR,
but for TRIP1,TRIP2,TRIP3,TRIP6, these are connected to input X-BAR. there are checking if these signal can connect to CMPSS?

what I am thinking is that these CMPSS signal like CTRIPH can connected to output X-bar and then GPIO pin, and the GPIO pin can be connected to input X-bar, then can go to ePWM module as TRIP1,TRIP2,TRIP3,TRIP6,
I am not sure if these can be done only by software, do they require to do PCB layout to connect GPIO of OUTPUTXBARx to another GPIO which used as input X-bar?