Part Number: TMS320F28076
Hi~
We are using the THVD1452DR chip to convert UART signals into 485 signals. We also have a 28076 device functioning as the master station and multiple 28076 devices as slave stations using SCI for communication. When Station A wants to transmit, the other slave stations need to pull down the DE pin of THVD1452DR. However, this action also causes the Rx signal of the master station to go to a low level, triggering the RXERROR flag. Is there any way to solve this issue?
Thanks in advance!
Best wishes,
Alan