This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C: [7/25/2023, 12:08:50 PM] [ERROR] C28xx_CPU1: File Loader: Verification failed: Values at address 0x000000@Program do not match Please verify target memory and memory map.

Part Number: TMS320F280039C
Other Parts Discussed in Thread: UNIFLASH

.Hello,

When running the UniFlash software and After successfully load the image of the f28003x_ucc5880.out

[7/25/2023, 12:08:44 PM] [SUCCESS] Program Load completed successfully.

When when trying to verify the Image, the following errors appears:

[7/25/2023, 12:08:50 PM] [ERROR] C28xx_CPU1: File Loader: Verification failed: Values at address 0x000000@Program do not match Please verify target memory and memory map.

Please see the attached screenshot.

  • Hi Alberto,

    I just confirmed that the verify was able to work using the LED blinky example. Could you try to load that .out and see if the same result occurs, as well as take a screenshot of the memory window? Also, I don't think the screenshot was attached. Please attach below if able.

    Thanks and regards,

    Charles