This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
There's an issue from the customer need your help:
Does the ROM of TMS320F28379D contain the content of sensorless control that can call the FAST library; whether the current Ti motor library has two forms: one is integrated with FAST in the ROM, which must be in 28062F, 280049C, 280025C, 280039C The other is the library of Ti's official motor laboratory, which can call the sensorless motor control content in all TiC2000 single-chip microcomputers.
Thanks & Regards,
Ben
Hi Ben,
I don't think the ROM of TMS320F28379D contain the content of sensorless control that can call the FAST library. If the customer wants to enable FAST sensorless control with F28379, he/she could leverage the fast lib in the libraries folder of motor control SDK as the universal motor control lab example with F280025/F280039.
Thanks,
Jiaxin