Part Number: TMS320F28P650DK
Hi Team,
I want to understand more on the ePWM X-BAR in F28P65x processor.
1. In the ePWM chapter, it is mentioned only about TRIP4 -12 (except for TRIP6) comes from ePWM XBAR.

However, in the ePWM XBAR chapter it is said the XBAR signal from ePWM XBAR A goes to TRIPIN 1 - 8 and ePWM XBAR B goes to TRIP9-15.

Although ePWM XBAR B has less output as per the image above, the registers for ePWM XBAR A and ePWM XBAR B are identical.
PFB my questions,
1. Are TRIPIN1-15 different from TRIP signals i.e TRIP1-12?
2. How are these signals mapped with each other?
3. Des OUT1 in ePWM Xbar A correspond to TRIPIN 1 and OUT1 in ePWM Xbar correspond to TRIPIN 9? If so then what is OUT8 in ePWM XBAR B?
4. Can I get more details on the enhancements of these XBARS from its predecessor 2838x?
Kind regards,
Irene