This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Hardware build in test in tms320f28379d

Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE

Hello everyone, first of all, I am new to these tasks, so I am open to your suggestions and examples.

I could not find a hwbıst example for tms320f28379d, can you tell me the file path if there is one?

tms320f28379d "C:\ti\c2000\C2000Ware_1_00_01_00\libraries\diagnostic\f2837xd\examples\cpu1\test_application" but I think this example is not related to HWBIST

I examined the HWBIST library and hwbist document, but I couldn't see an example, can you tell me if there is an example?

  • You have the correct path listed above for the diagnostics library.  The example code will execute all static tests, including the HWBIST.  If you look at the sta_test.c file in the same directory you will see an enumeration for both the HWBIST_full and the HWBIST_micro.  I believe it is tests 6 and 7, in terms of passing those into the general function if you don't want to run the other tests included.

    Best,

    Matthew

  • Hi Mathew

     I didn't think that hwbist in test application tests example all hwbist content if so thank you