This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Having a severe problem in developing our pulse width modulator, I have set the TBPRD to 1200 such that the frequency is around 166kHz. However on my scope I am seeing my switching waveform at just 10kHz.
Here is the code for this part of the controller:
void initEPWM1(void) {
// Set up time-base clock.
EPWM_setTimeBasePeriod(EPWM1_BASE, EPWM_TIMER_TBPRD);
EPWM_setPhaseShift(EPWM1_BASE, 0);
EPWM_setTimeBaseCounter(EPWM1_BASE, 0);
// Counter compare config for EPWM1. May just need CMPA if use FED/RED.
EPWM_setCounterCompareValue(EPWM1_BASE,
EPWM_COUNTER_COMPARE_A,
EPWM_TIMER_TBPRD/2);
EPWM_setCounterCompareValue(EPWM1_BASE,
EPWM_COUNTER_COMPARE_B,
EPWM_TIMER_TBPRD/2);
// Set up counter mode.
EPWM_setTimeBaseCounterMode(EPWM1_BASE, EPWM_COUNTER_MODE_UP);
EPWM_disablePhaseShiftLoad(EPWM1_BASE);
EPWM_setClockPrescaler(EPWM1_BASE,
EPWM_CLOCK_DIVIDER_2,
EPWM_HSCLOCK_DIVIDER_2);
// Set up PWM Shadowing. Load on CTR ZRO.
EPWM_setCounterCompareShadowLoadMode(EPWM1_BASE,
EPWM_COUNTER_COMPARE_A,
EPWM_COMP_LOAD_ON_CNTR_ZERO);
EPWM_setCounterCompareShadowLoadMode(EPWM1_BASE,
EPWM_COUNTER_COMPARE_B,
EPWM_COMP_LOAD_ON_CNTR_ZERO);
// Set up the action qualifier.
EPWM_setActionQualifierAction(EPWM1_BASE,
EPWM_AQ_OUTPUT_A,
EPWM_AQ_OUTPUT_HIGH,
EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO);
EPWM_setActionQualifierAction(EPWM1_BASE,
EPWM_AQ_OUTPUT_B,
EPWM_AQ_OUTPUT_LOW,
EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO);
EPWM_setActionQualifierAction(EPWM1_BASE,
EPWM_AQ_OUTPUT_A,
EPWM_AQ_OUTPUT_LOW,
EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
EPWM_setActionQualifierAction(EPWM1_BASE,
EPWM_AQ_OUTPUT_B,
EPWM_AQ_OUTPUT_HIGH,
EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
// Interrupt where we will change execute control code.
// Select INT on time base counter zero event
// Enable INT, but generate on the 15th event
// Bandwidth is then FSW/15.
EPWM_setInterruptSource(EPWM1_BASE, EPWM_INT_TBCTR_ZERO);
EPWM_enableInterrupt(EPWM1_BASE);
EPWM_setInterruptEventCount(EPWM1_BASE, 15);
}
void initEPWM2(void) {
// Set up time-base clock.
EPWM_setTimeBasePeriod(EPWM2_BASE, EPWM_TIMER_TBPRD);
// Initially zero, but test with different TBPHS.
// Ensure Time base is set to same value as phase shift.
EPWM_setPhaseShift(EPWM2_BASE, 300);
EPWM_setTimeBaseCounter(EPWM2_BASE, 300);
// Counter compare config for EPWM2. May just need CMPA if use FED/RED.
EPWM_setCounterCompareValue(EPWM2_BASE,
EPWM_COUNTER_COMPARE_A,
EPWM_TIMER_TBPRD/2);
EPWM_setCounterCompareValue(EPWM2_BASE,
EPWM_COUNTER_COMPARE_B,
EPWM_TIMER_TBPRD/2);
// Set up counter mode.
EPWM_setTimeBaseCounterMode(EPWM2_BASE, EPWM_COUNTER_MODE_UP);
EPWM_disablePhaseShiftLoad(EPWM2_BASE);
EPWM_setClockPrescaler(EPWM2_BASE,
EPWM_CLOCK_DIVIDER_2,
EPWM_HSCLOCK_DIVIDER_2);
// Set up PWM Shadowing. Load on CTR ZRO.
EPWM_setCounterCompareShadowLoadMode(EPWM2_BASE,
EPWM_COUNTER_COMPARE_A,
EPWM_COMP_LOAD_ON_CNTR_ZERO);
EPWM_setCounterCompareShadowLoadMode(EPWM2_BASE,
EPWM_COUNTER_COMPARE_B,
EPWM_COMP_LOAD_ON_CNTR_ZERO);
// Set up the action qualifier.
// Scope these and check if right, most likely need to be different to EPWM1.
EPWM_setActionQualifierAction(EPWM2_BASE,
EPWM_AQ_OUTPUT_A,
EPWM_AQ_OUTPUT_HIGH,
EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO);
EPWM_setActionQualifierAction(EPWM2_BASE,
EPWM_AQ_OUTPUT_B,
EPWM_AQ_OUTPUT_LOW,
EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO);
EPWM_setActionQualifierAction(EPWM2_BASE,
EPWM_AQ_OUTPUT_A,
EPWM_AQ_OUTPUT_LOW,
EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
EPWM_setActionQualifierAction(EPWM2_BASE,
EPWM_AQ_OUTPUT_B,
EPWM_AQ_OUTPUT_HIGH,
EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
// Interrupt where we will change execute control code.
// Select INT on time base counter zero event
// Enable INT, but generate on the 15th event
// Bandwidth is then FSW/15.
EPWM_setInterruptSource(EPWM2_BASE, EPWM_INT_TBCTR_ZERO);
EPWM_enableInterrupt(EPWM2_BASE);
EPWM_setInterruptEventCount(EPWM2_BASE, 15);
}
void setupEPWMActiveHighComplementary() {
// As always, use EPWMA as the input for both RED and FED.
EPWM_setRisingEdgeDeadBandDelayInput(EPWM1_BASE, EPWM_DB_INPUT_EPWMA);
EPWM_setRisingEdgeDeadBandDelayInput(EPWM2_BASE, EPWM_DB_INPUT_EPWMA);
EPWM_setFallingEdgeDeadBandDelayInput(EPWM1_BASE, EPWM_DB_INPUT_EPWMA);
EPWM_setFallingEdgeDeadBandDelayInput(EPWM2_BASE, EPWM_DB_INPUT_EPWMA);
// Set the rising and falling edge delay values. One percent of switching period, for now.
EPWM_setFallingEdgeDelayCount(EPWM1_BASE, EPWM_TIMER_TBPRD/100);
EPWM_setFallingEdgeDelayCount(EPWM2_BASE, EPWM_TIMER_TBPRD/100);
EPWM_setRisingEdgeDelayCount(EPWM1_BASE, EPWM_TIMER_TBPRD/100);
EPWM_setRisingEdgeDelayCount(EPWM2_BASE, EPWM_TIMER_TBPRD/100);
// Invert only the falling edge delayed output for active-high complementary mode.
EPWM_setDeadBandDelayPolarity(EPWM1_BASE, EPWM_DB_RED, EPWM_DB_POLARITY_ACTIVE_HIGH);
EPWM_setDeadBandDelayPolarity(EPWM1_BASE, EPWM_DB_FED, EPWM_DB_POLARITY_ACTIVE_LOW);
EPWM_setDeadBandDelayPolarity(EPWM2_BASE, EPWM_DB_RED, EPWM_DB_POLARITY_ACTIVE_HIGH);
EPWM_setDeadBandDelayPolarity(EPWM2_BASE, EPWM_DB_FED, EPWM_DB_POLARITY_ACTIVE_LOW);
// Use the delayed signals instead of the original signals.
EPWM_setDeadBandDelayMode(EPWM1_BASE, EPWM_DB_RED, true);
EPWM_setDeadBandDelayMode(EPWM1_BASE, EPWM_DB_FED, true);
EPWM_setDeadBandDelayMode(EPWM2_BASE, EPWM_DB_RED, true);
EPWM_setDeadBandDelayMode(EPWM2_BASE, EPWM_DB_FED, true);
// Importantly, do not switch output A with output B.
EPWM_setDeadBandOutputSwapMode(EPWM1_BASE, EPWM_DB_OUTPUT_A, false);
EPWM_setDeadBandOutputSwapMode(EPWM1_BASE, EPWM_DB_OUTPUT_B, false);
EPWM_setDeadBandOutputSwapMode(EPWM2_BASE, EPWM_DB_OUTPUT_A, false);
EPWM_setDeadBandOutputSwapMode(EPWM2_BASE, EPWM_DB_OUTPUT_B, false);
}
EPWM2 is set up the exact same way as EPWM with just a variable phase shift, but also switches at just 10kHz.
Could anyone point me in the direction for what may be happening here?
Best regards,
JMH
Hi JMH,
EPWM_setClockPrescaler(EPWM1_BASE,
EPWM_CLOCK_DIVIDER_2,
EPWM_HSCLOCK_DIVIDER_2);
Assuming your SYSCLK is 200Mhz, and EPWMCLKDIV is /2, you're dividing by EPWM_CLOCK_DIVIDER_2 and EPWM_HSCLOCK_DIVIDER_2, thus dividing this clock to a value of 200Mhz / 8 =25Mhz. Is this correct? If you are wanting this in counter up mode, you can use the formula provided within the TRM.
EPWM_setTimeBaseCounterMode(EPWM1_BASE, EPWM_COUNTER_MODE_UP);
I am getting a value of 150 for the TBPRD for a 166kHz signal, assuming that TBCLK is in fact 25MHz.
Best,
Ma
Didn’t realise that the HS clock divider had that effect.
Preferably for maximum duty cycle resolution we would want to use the PWM clock at its maximum speed so around 100MHz if I remember correctly.
Can you suggest an alternative call to the function setClockPrescaler that allows us to run at 100MHz? I just took this example from one of the driverlib projects and didn’t expect it to divide the signal down by such a high value.
thanks for your help!
Hi JM,
Yes I would suggest setting the the clock pre scalers to all /1. Since SYSCLK is 200Mhz, and PERCLKDIVSEL will /2 by default. You can set the other prescalers to be /1. This will give you the 100Mhz max speed to the PWM clock.
EPWM_setClockPrescaler(EPWM1_BASE,
EPWM_CLOCK_DIVIDER_1,
EPWM_HSCLOCK_DIVIDER_1);
Best,
Ma