Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800137: UART RXSHF -> SCIRXBUF condition

Part Number: TMS320F2800137

Hi,
I have some general questions.

The data will only transfered from RXSHF to SCIXBUF if no receive error RXERROR (bits 5-2: BRKDT, FE, OE, and PE) occurs, ok?

RXSHF begin receiving with the start bit? What is the condition to detect a start bit? Long time high (how many SCICLK???) followed by by four consecutive
internal SCICLK periods of zero bits.

After an detected error the RXSHF will be cleared? At each new start bit the RXSHF will be cleared?

Two bit error can't be detected, right?

Regards, Holger

  • Hi Holger,

    RXSHF begin receiving with the start bit? What is the condition to detect a start bit? Long time high (how many SCICLK???) followed by by four consecutive
    internal SCICLK periods of zero bits.

    This is mentioned in the SCI TRM Chapter:

    All other items are mentioned in the various register descriptions of each of the items you mentioned. If you have questions on specific wordings in the TRM registers, please let me know, and provide screenshots of what you have confusion on.

    Regards,

    Vince

  • it would be easier you had quickly answered my questions instead of the hint RTFM

  • My apologies, did not mean for it to come across that way.

    Here are the direct answers to your questions:

    The data will only transfered from RXSHF to SCIXBUF if no receive error RXERROR (bits 5-2: BRKDT, FE, OE, and PE) occurs, ok?

    Yes, however data should transfer regardless into RXSHF FROM PIN unless there is something disabling the RXENA bit.

    RXSHF begin receiving with the start bit? What is the condition to detect a start bit? Long time high (how many SCICLK???) followed by by four consecutive
    internal SCICLK periods of zero bits.

    Yes. Condition is 4 low SCICLK periods. The high period does not matter in this case as long as it is greater than 1 bit. 2 stop bits of high is recommended.

    After an detected error the RXSHF will be cleared? At each new start bit the RXSHF will be cleared?

    Other than new start bit, RXSHF will not get cleared unless SCI reset occurs, or the data is shifted into the fifo/buffer. RXSHF clears on new start bit.

    Two bit error can't be detected, right?

    Correct.

  • thanks, Vince.