This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SCI FIFO RX interrupt not triggering



Hi all,

I'm having trouble getting the SCIRX FIFO interrupt to trigger when it seems it should be.  I'm using the SCI-C module on a TMS320F2335.

I have the SCI-C RX FIFO register configured as such:

ScicRegs.SCIFFRX.all = 0x0061;

Which I believe should trigger an interrupt when the FIFO level is 1 or greater.

I think I have the interrupt configured properly in my main() function...

DINT;

InitPieCtrl();

IER = 0x0000;

IFR = 0x0000;

InitPieVectTable();

EALLOW;

PieVectTable.SCIRXINTC = &scicRxFifoIsr;

EDIS;

IER |= M_INT8;

PieCtrlRegs.PIECTRL.bit.ENPIE = 1;

PieCtrlRegs.PIEIER8.bit.INTx5 = 1;

EINT;

...but let me know if something looks amiss.  SCI-C RX is definitely receiving data, but no interrupt is generated.

Thanks so much for any and all help!

-sam