This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Champs,
I ask this for our customer.
My customer finds that the flash .cmd in C2000WARE use ALIGN(8) for flash memory. He wants to change it to align(4). He has following questions about that:
1. In order to change it to ALIGN(4), could we just replace all "ALIGN(8)" with “ALIGN(4)”? Is there any risk if we use ALIGN(4)? Such as affect the alignment of FLASH API?
2. Could he use both ALIGN(4) and ALIGN(8) in .cmd?
Best Regards
Kita
Hi Kita,
Understood. Then, the customer needs to ensure that the flash programmers that they use (custom or 3rd party) can program 64-bits at-a-time.
Thanks and regards,
Vamsi