This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Dead band unstable when the value of the high resoltion period register (TBPRDHR) is non-zero.

Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE, SYSCONFIG

Hello, I'm new to programming on microcontrollers. I use : TMS320F28379D. I code on CCS. I'm looking to make a PWM signal (high resolution) at 50% duty cycle with a dead band in active complentary on up count mode  on F2837xD.

The PWM signal works perfectly with 50% duty cycle when the deadband is deactivated (HRPE on). But when dead band is on, my PWM signal is not stable.
There are two cases with dead band:
 -  First, when the high-resolution period is activated and  TBPRDHR = 0 <<8. The signal is stable, the dead band is working. Example : Periode=210ns, so TBPRD = 20, TBPRDHR = 0 and  105ns of duty cycle.
 -  Second, when the high-resolution period is activated and  TBPRDHR is non-zero, the signal is not stable. Example : Periode 206ns, so TBPRD = 19, TBPRDHR = 0.6 <<8 and duty cycle = 103ns.


I observed a 10 ns variation (1 TBCLK). I also observe that the EPwm1B signal is stable, but not the EPw1A signal when the trigger is on the Epwm1B's chanel. But not on the EPw1A's chanel, both of them are unstable.
I don't know how to stabilize the signal.
Thank you in advance for your help.

Here are photos of the signal and the difference in variation (Chanel 1 : Epwm1B and chanel 2 : Epwm1A), the pictures represent a PWM signal with 206ns period, dutycycle 50% and deadband of 30% of the demi periode (30.9ns) :

Continuous signal acquisition :

Single acquisition  :

Here is my complete code if it helps:

#include "F28x_Project.h"
#include "F2837xD_device.h"
#include "F2837xD_Examples.h"
#include "F2837xD_EPwm_defines.h"                       // init defines
#include "SFO_V8.h"
#include "board.h"
#include <stdio.h>




float PeriodeNANOsec = 206;                             //Periode souhaité en NANOSECONDE
float dutycycle = 0.5;
float dutyDB = 0.30;                                    //DN(ns)= dutyDB * Periode/2

            //--------------  DEFINITION  --------------//
#define LAST_EPWM_INDEX     4

            //---------------- VARIABLE ----------------//
uint16_t PRD1_HR;
uint16_t FED;
uint16_t FEDHR;
uint16_t PRD;
uint16_t CMP;
uint16_t CMPHR;


            //--------------  GLOBAL  ------------------------//
int MEP_ScaleFactor;
volatile struct EPWM_REGS *ePWM[] = {0, &EPwm1Regs, &EPwm2Regs, &EPwm3Regs};
uint16_t status;
float DBns;
            //---- APPEL DE FONCTION----//
void PRD_CMP_DB_calculation(float32_t periode, float32_t duty,float32_t dutyDB);    //calculation of PRD, CMP and DB values (high resolution)
void initGPIO(void);                                                                                                        //GPIO initialization
void initPWM(void);                                                                                                        //PWM initialization


            //****************** CODE PRINCIPAL***********************//
int main()
{
    PRD_CMP_DB_calculation(PeriodeNANOsec,dutycycle,dutyDB);
    DBns = dutyDB * PeriodeNANOsec/2;
    // Initialize System Control for Control and Analog Subsystems
    // Enable Peripheral Clocks
    EALLOW;
    InitSysCtrl();
    EDIS;

    // EPWM1A and EPWM1B through all PWMS
    initGPIO();
    DINT;

    // Initialize PIE control registers to their default state.
    // The default state is all PIE interrupts disabled and flags
    // are cleared.
    InitPieCtrl();

    // Disable CPU interrupts and clear all CPU interrupt flags:
    EALLOW;
    IER = 0x0000;
    IFR = 0x0000;

    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    // This will populate the entire table, even if the interrupt
    // is not used in this example.  This is useful for debug purposes.
    // The shell ISR routines are found in F2837xD_DefaultIsr.c.
    // This function is found in F2837xD_PieVect.c.
    InitPieVectTable();

    // Enable global Interrupts and higher priority real-time debug events:
    EINT;   // Enable Global interrupt INTM
    ERTM;   // Enable Global realtime interrupt DBGM

    // Calling SFO() updates the HRMSTEP register with calibrated MEP_ScaleFactor.
    // HRMSTEP must be populated with a scale factor value prior to enabling
    // high resolution period control.
    while(status == SFO_INCOMPLETE)
    {
        status = SFO();                                         // SFO function returns 2 if an error occurs & # of MEP
        if(status == SFO_ERROR)                                 // steps/coarse step exceeds maximum of 255.
        {
            ESTOP0;
        }
    }

    SysCtl_disablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);

    initPWM();

    SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
    uint32_t i;

    while(1)
    {


        for(i=1; i<LAST_EPWM_INDEX; i++)
        {
            (*ePWM[i]).TBPRDHR= PRD1_HR<<8;
        }
        status = SFO(); // in background, MEP calibration module
        // continuously updates MEP_ScaleFactor
        if(status == SFO_ERROR)
        {
            ESTOP0;   // SFO function returns 2 if an error occurs & # of
        }              // MEP steps/coarse step exceeds maximum of 255.

    }
}

         //------------------ INITIALISATION HRPWM    -------------//
void initPWM()
{
    uint16_t j;

    EALLOW;
    CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 0;                           // Disable TBCLK within the EPWM
    EDIS;

    for(j=1; j<LAST_EPWM_INDEX; j++)
    {
        //------------------    TIME BASE/ CMP  --------------------//
        (*ePWM[j]).TBCTL.bit.PRDLD = TB_SHADOW;                     // set Shadow load
        (*ePWM[j]).TBPRD= PRD;                                      // PWM frequency = 1/(2*TBPRD))

        (*ePWM[j]).CMPA.all = (long) CMP << 16 | CMPHR << 8;         //Enable HRPWM duty
        (*ePWM[j]).CMPB.all = (long) CMP << 16 | CMPHR << 8;

        (*ePWM[j]).TBPHS.all = 0;
        (*ePWM[j]).TBCTR = 0;

        (*ePWM[j]).TBCTL.bit.CTRMODE = TB_COUNT_UP;                 // Select up-down count mode
        (*ePWM[j]).TBCTL.bit.SYNCOSEL = TB_SYNC_DISABLE;
        (*ePWM[j]).TBCTL.bit.HSPCLKDIV = TB_DIV1;
        (*ePWM[j]).TBCTL.bit.CLKDIV = TB_DIV1;                      // TBCLK = SYSCLKOUT
        (*ePWM[j]).TBCTL.bit.FREE_SOFT = 3;

        //--------------------    SHADOWS  -------------------------//
        (*ePWM[j]).CMPCTL.bit.LOADAMODE = CC_CTR_PRD;               // LOAD CMPA on CTR = PRD
        (*ePWM[j]).CMPCTL.bit.LOADBMODE = CC_CTR_PRD;
        (*ePWM[j]).CMPCTL.bit.SHDWAMODE = CC_SHADOW;
        (*ePWM[j]).CMPCTL.bit.SHDWBMODE = CC_SHADOW;

        //------------------    ACTION QUALIFIER -------------------//

        (*ePWM[j]).AQCTLA.bit.CAU = AQ_CLEAR;                       // PWM toggle high/low
        (*ePWM[j]).AQCTLA.bit.PRD = AQ_SET;                         //DO NOT SET TO ZRO, HR period is not stable
        //(*ePWM[j]).AQCTLB.bit.CBU = AQ_SET;                       // PWM toggle high/low
        //(*ePWM[j]).AQCTLB.bit.PRD = AQ_CLEAR;

        //---------------------    HRPWM  --------------------------//
        EALLOW;
        (*ePWM[j]).HRCNFG.all = 0x0;

        (*ePWM[j]).HRCNFG.bit.EDGMODE = HR_BEP;                     // BOht Edge for the HR period to work
        (*ePWM[j]).HRCNFG.bit.CTLMODE = HR_CMP;                     // CMPAHR and TBPRDHR HR control.
        (*ePWM[j]).HRCNFG.bit.HRLOAD = HR_CTR_ZERO_PRD;             // load on CTR = 0  and CTR = TBPRD

        (*ePWM[j]).HRCNFG.bit.EDGMODEB = HR_BEP;                    // BOht Edge for the HR period to work
        (*ePWM[j]).HRCNFG.bit.CTLMODEB = HR_CMP;                    // CMPBHR and TBPRDHR   HR control
        (*ePWM[j]).HRCNFG.bit.HRLOADB = HR_CTR_ZERO_PRD;            // load on CTR = 0  and CTR = TBPRD
        (*ePWM[j]).HRCNFG.bit.SWAPAB = 0;                           // ePWMxA and ePWMxB outputs are unchanged

        (*ePWM[j]).HRCNFG.bit.AUTOCONV = 1;                         // Enable autoconversion for HR period
        (*ePWM[j]).HRPCTL.bit.TBPHSHRLOADE = 0;                     // Enable TBPHSHR sync  (required for updwn count HR control)
        (*ePWM[j]).HRPCTL.bit.HRPE = 1;                             // Turn on high-resolution period control.

        CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1;                       // Enable TBCLK within the EPWM
        (*ePWM[j]).TBCTL.bit.SWFSYNC = 1;                           // Synchronize high resolution phase to start HR period

        //--------------------    DEAD BAND  -----------------------//
        (*ePWM[j]).DBCTL.bit.IN_MODE = DBA_ALL;                     //ICI EPWMxA est la source des retards de front descendant et de front montant.
        (*ePWM[j]).DBCTL.bit.OUT_MODE= DB_FULL_ENABLE ;             // See table 15-8
        (*ePWM[j]).DBCTL.bit.POLSEL= DB_ACTV_HIC;                   //Active High Complementary -> tableau 15-8
        (*ePWM[j]).DBCTL.bit.HALFCYCLE= 1;                          //this bit must be set 1 for HR deadband (clock 5ns for DB)
        (*ePWM[j]).DBCTL.bit.OUTSWAP = 0;
        (*ePWM[j]).DBCTL.bit.SHDWDBREDMODE = 1;
        (*ePWM[j]).DBCTL.bit.SHDWDBFEDMODE = 1;
        (*ePWM[j]).DBCTL.bit.LOADREDMODE = 2;
        (*ePWM[j]).DBCTL.bit.LOADFEDMODE = 2;
        (*ePWM[j]).DBRED.all = FED;                                 //Unpacking the assembly
        (*ePWM[j]).DBFED.all = FED;
        (*ePWM[j]).HRCNFG2.bit.EDGMODEDB= HR_BEP;                   // DBREDHR and DBFEDHR
        (*ePWM[j]).HRCNFG2.bit.CTLMODEDBFED =2;                     // Load on ZRO
        (*ePWM[j]).HRCNFG2.bit.CTLMODEDBRED =2;
        (*ePWM[j]).DBREDHR.bit.DBREDHR = FEDHR;                     //Unpacking the ascent of the two PW1Ms
        (*ePWM[j]).DBFEDHR.bit.DBFEDHR = FEDHR;                     //Unpacking the descent of the two PW1Ms


        EDIS;


    }
}


        //------------------ INITIALISATION GPIO      --------------//
void initGPIO()
{
    EALLOW;                                                 // Enable access to GPIO configuration registers
    // CONFIGURE GPIO 0 FOR PWM1A
    GpioCtrlRegs.GPAPUD.bit.GPIO0 = 0;                      // Activate pull-up resistor on pin
    GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1;                     // Configure pin for PWM1A function
    // CONFIGURE GPIO 1 FOR PWM1B
    GpioCtrlRegs.GPAPUD.bit.GPIO1 = 0;                      // Activate pull-up resistor on pin
    GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1;                     // Configure pin for PWM1B function
    EDIS;                                                   // Disable access to GPIO configuration registers
}


void PRD_CMP_DB_calculation(float32_t periode, float32_t duty,float32_t dutyDB)
{
        //--------- Period and PRDHR calculation  ----------//
   float invTBCLK= 0.10;                                    //1/TBCLK = 0.1 nanosec, Number of clock strokes with TBCLK=10ns
   float PRDfrac=periode*invTBCLK;                          //Flaot number of TBCLK for the p
   int PRDint=(PRDfrac);                                    //the integer part of the split period
       PRD=PRDint-1;
       PRD1_HR=(PRDfrac-PRDint)*256;

       //---------- CMP and CMPHR  calculation  ------------//
   int reste = PRD/2;                                       //Euclidean division to find out how to calculate CMP at 50%duty
   if (reste !=0)                                           //If PRd is Odd
   {
       CMP=PRDint/2 - 1;
   }
   else                                                     //If PRD is even
   {
       CMP=PRD/2;
   }
   float frac = PRDfrac*duty;                               //calculation of CMPHR = frac(PRDfrc*duty)
   int ent = (frac);
   float CMPHRfrac = frac-ent;
   CMPHRfrac = CMPHRfrac*256;
   CMPHR=(CMPHRfrac);

       //---------- Dead Band and DBHR calculation  --------//
   float RequiredDBvalue=duty*periode*dutyDB;
   float fracFED=RequiredDBvalue*0.2;                       //*0.2 is equivalent to dividing by 10ns/2 or half a clock cycle
   FED=(fracFED);
   float fracFEDHR= (fracFED-FED)*128;                      //DBFED is on 7 bits so for the cacul we realize the (fractionalpart*128)
   FEDHR=(fracFEDHR);
}

  • Hi Florentin,

    Thank you for sending the scope shots and code. The +/- 1 TBCLK jitter is usually a symptom of some incompatible settings with HRPWM. The big issue I see right now is that your count mode is not compatible with what you are trying to configure. If you are trying to have MEP control of both edges for your EPWMA/B, then you must use up-down-count mode. MEP edge control of both edges is not supported for up-count mode, which is what you currently have configured. If you are in up-count mode, the Dead Band module is also not supported in HR mode. So I would recommend switching to up-down count mode for this program.

    Some other notes to check:

    • If you change to up-down-count mode and are doing both edge control, then in this case you need to have action qualifier settings as follows:
      • CMPxUp = set
      • CMPxDown = clear
      • No actions on TBCTR = PRD or TBCTR = ZRO
    • Also, if you want to enable HR Period control, make sure both channels (A and B) have it enabled otherwise the non-HR output will have +/- 1 TBCLK cycle jitter.

    If you haven't already referenced out software examples, I would recommend you also take a look at the HRPWM examples we have at {C2000Ware}\device_support\f2837xd\examples\cpu1\ and C:\ti\c2000\C2000Ware_5_01_00_00\driverlib\f2837xd\examples\cpu1\hrpwm. These can be good to use as guidance when setting up your HRPWM configurations. As a side note: Using the SysConfig GUI in CCS would also catch many of these settings and warn you about incompatibilities as well if you are interested in developing that wayBlush.

    Best Regards,

    Allison

  • Thank you for your help and your answer.

    I configured my signal in up/down count and after modifying my period and duty cycle calculations, the signal is stable when the dead band is active (with the expected values).


    Thanks again,
    Best Regards,

    Florentin