This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Is it possible to enable both TBPRDHR and CMPAHR at the same time?

Expert 2570 points
Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE

Hi All,

Is it possible to enable both TBPRDHR and CMPAHR at the same time?

TBPRDHR and CMPAHR are as described in TRM "15.14.1.3 HRPWM Settings",
However, it seems that only TBPRDHR and CMPAHR can be selected in "Edge Mode".
Therefore, as far as TRM is concerned, it is not possible to enable both at the same time.

Best Regards,

Ito

  • Hi Ito,

    Yes, you can enable both TBPRDHR and CMPAHR by using the "both edge mode" and enabling period control. I see that some of the register descriptions are a bit confusing and am working on updating these. 

    Best Regards,

    Allison

  • Hi Allison

    Thank you for your reply.

    I also tried setting Both Edges (BE) but it did not reflect CMPAHR.
    I have the impression that there are other settings that are needed,
    such as whether to use up-down count mode or the AQ module settings.
    If you know the detailed settings for PWM to enable both TBPRDHR and CMPAHR, please let me know.

    Best Regards,

    Ito

  • Hi Ito,

    Let me check to see if we have some existing examples on this that you can use Slight smile

    Best Regards,

    Allison

  • Hi Ito,

    I just put together some code using our existing examples to implement duty control and period control in a highly simplified manner. Only EPWM1 module is used (both channel A and B), CMPxHR values are left constant (able to be changed by the user), and TBPRDHR is very slowly incremented.

    I'd recommend you import an existing example (such as {C2000Ware}\driverlib\f2837xd\examples\cpu1\hrpwm\hrpwm_ex4_duty_updown_sfo) into CCS and then replace the hrpwm_ex4_duty_updown_sfo.c file contents with what I have below. Hope this helps show what settings you should implement!

    //#############################################################################
    //
    // FILE:   hrpwm_simple_duty_and_period_control_updown_sfo.c
    //
    // TITLE:  HRPWM DUTY and PERIOD CONTROL (simplified).
    //
    //#############################################################################
    //
    // This is a simplified HRPWM example where HRPWM duty control and
    // HRPWM period control capability are both already set up for you on only
    // one PWM module (EPWM1). This example uses CMPAHR, CMPBHR, and TBPRDHR to show the
    // implementation of HR duty and period modulation together. The user can alter
    // CMPAHR and CMPBHR values during run time in the register viewing window of CCS.
    // the example slowly increments the TBPRDHR value to increase the TBPRDHR value.
    // You can see the outputs of channels EPWM1A and EPWM1B change on an oscilloscope.
    // Increasing CMPxHR values will decrease the duty cycle of channel 'x'.
    // The incrementing of TBPRDHR will lower the frequency by lengthening the period of both channels.
    //
    // Period is incremented by default. To adjust the duty cycle while running the code:
    // 1. Open the Registers window in CCS.
    // 2. Turn on Continuous Refresh using the yellow arrows button.
    // 3. Scroll to EPWM1 registers and expand them.
    // 4. Find the CMPA and CMPB registers. Click the arrow to expand them so you see the HR elements.
    // 5. Right-click on CMPAHR and CMPBHR and change the number formats to Hex for readability.
    // 6. Double-click on the CMPAHR or CMPBHR register and change the value from 0x0100 to 0xFF00.
    // This changes the CMPxHR value from 1 to the max (255). Maxing out CMPxHR to 255 should result
    // in a 1-clock-cycle change.
    //
    // From here, you can continue to alter the HR numbers as needed for HR duty and period control.
    //
    //
    //#############################################################################
    //
    // Included Files
    //
    #include "driverlib.h"
    #include "device.h"
    #include "board.h"
    #include "SFO_V8.h"
    
    //
    // Defines
    //
    #define EPWM_TIMER_TBPRD    100UL           // TBPRD value for this example is set to 100
    #define LAST_EPWM_INDEX_FOR_EXAMPLE    2    // Used for the EPWM initialization function
    
    //
    // Globals
    //
    
    float32_t periodFine = 0.20; //HRPWM period percentage
    uint16_t status;
    
    int MEP_ScaleFactor; // Global variable used by the SFO library
                         // Result can be used for all HRPWM channels
                         // This variable is also copied to HRMSTEP
                         // register by SFO() function.
    
    //
    // Store the EPWM1 'base' name here (can append other EPWM modules as needed)
    //
    volatile uint32_t ePWM[] = {0, myEPWM1_BASE};
    
    //
    // Function Prototypes
    //
    void initHRPWM(uint32_t period);
    void error(void);
    __interrupt void epwm1ISR(void);
    
    
    //
    // Main
    //
    void main(void)
    {
        //
        // Initialize device clock and peripherals
        //
        Device_init();
    
        //
        // Disable pin locks and enable internal pull ups.
        //
        Device_initGPIO();
    
        //
        // Initialize PIE and clear PIE registers. Disables CPU interrupts.
        //
        Interrupt_initModule();
    
        //
        // Initialize the PIE vector table with pointers to the shell Interrupt
        // Service Routines (ISR).
        //
        Interrupt_initVectorTable();
    
        //
        // Assign the interrupt service routines to ePWM interrupts
        //
        Interrupt_register(INT_EPWM1, &epwm1ISR);
    
    
        //
        // Initialize the EPWM GPIOs and change XBAR inputs from using GPIO0
        // This will implement any SysConfig configurations. Note that any configurations
        // that occur after this will overwrite your SysConfig configurations.
        //
        Board_init();
    
        //
        // Calling SFO() updates the HRMSTEP register with calibrated MEP_ScaleFactor.
        // HRMSTEP must be populated with a scale factor value prior to enabling
        // high resolution period control.
        //
        while(status == SFO_INCOMPLETE)
        {
            status = SFO();
            if(status == SFO_ERROR)
            {
                error();   // SFO function returns 2 if an error occurs & # of MEP
            }              // steps/coarse step exceeds maximum of 255.
        }
    
        //
        // Disable sync(Freeze clock to PWM as well)
        //
        SysCtl_disablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
    
    
        //
        // Initialize the EPWM1 module in code with PRD set to EPWM_TIMER_TBPRD (in this example, 100)
        //
        initHRPWM(EPWM_TIMER_TBPRD);
    
        //
        // Enable sync and clock to PWM
        //
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
    
    
        // Enable ePWM interrupts
        //
        Interrupt_enable(INT_EPWM1);
    
    
        //
        // Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
        //
        EINT;
        ERTM;
    
    
        for(;;)
        {
            //
            // Apply HRPWM Period Control (slowly increments 0.2 to 0.9 in 0.1 steps, then starts over)
            //
            for(periodFine = 0.2; periodFine < 0.9; periodFine += 0.1)
            {
                DEVICE_DELAY_US(1000000);
                uint16_t i = 0;
    
                for(i=1; i<LAST_EPWM_INDEX_FOR_EXAMPLE; i++)
                {
                    float32_t count = ((EPWM_TIMER_TBPRD-1) << 8UL) + (float32_t)(periodFine * 256);
                    uint32_t compCount = count;
                    HRPWM_setTimeBasePeriod(ePWM[i], compCount);
                }
    
                //
                // Call the scale factor optimizer lib function SFO()
                // periodically to track for any change due to temp/voltage.
                // This function generates MEP_ScaleFactor by running the
                // MEP calibration module in the HRPWM logic. This scale
                // factor can be used for all HRPWM channels. The SFO()
                // function also updates the HRMSTEP register with the
                // scale factor value.
                //
                status = SFO(); // in background, MEP calibration module
                                     // continuously updates MEP_ScaleFactor
    
                if (status == SFO_ERROR)
                {
                    error();   // SFO function returns 2 if an error occurs & #
                                    // of MEP steps/coarse step
                }              // exceeds maximum of 255.
            }
        }
    }
    
    //
    // Define the EPWM1 ISR
    //
    __interrupt void epwm1ISR(void)
    {
        //
        // This is left empty for the user to fill as needed
        //
    
        EPWM_clearEventTriggerInterruptFlag(EPWM1_BASE); // Clear the interrupt flag from the PWM module
        Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP3); // Acknowledge the EPWM interrupt group in the PIE to reset the ACK bit
    }
    
    //
    // Initialize your EPWM1 module as with HR configurations (PRD is function input)
    //
    void initHRPWM(uint32_t period)
    {
        uint16_t j;
    
        // Parse through all EPWM modules you want this to apply to. In this case, only EPWM1 will be initalized.
    
        for (j=1;j<LAST_EPWM_INDEX_FOR_EXAMPLE;j++)
        {
            //
            // Set PWM mode to free run so that debugger does not stop it
            //
            EPWM_setEmulationMode(ePWM[j], EPWM_EMULATION_FREE_RUN);
    
            //
            // Set-up TBCLK
            //
            EPWM_setPeriodLoadMode(ePWM[j], EPWM_PERIOD_SHADOW_LOAD);
            EPWM_setTimeBasePeriod(ePWM[j], period-1);
            EPWM_setPhaseShift(ePWM[j], 0U);
            EPWM_setTimeBaseCounter(ePWM[j], 0U);
    
            //
            // Set up base duty to be 50% (CMPx = 50, TBPRD = 100)
            // Initialize CMPxHR values to be 1 (these are within the CMPA and CMPB registers, but must be written to in a particular way as shown below.
            //
            HRPWM_setCounterCompareValue(ePWM[j], HRPWM_COUNTER_COMPARE_A, (period/2 << 8) + 1);
            HRPWM_setCounterCompareValue(ePWM[j], HRPWM_COUNTER_COMPARE_B, (period/2 << 8) + 1);
    
    
            //
            // Set up counter mode to be up-down counter mode
            //
            EPWM_setTimeBaseCounterMode(ePWM[j], EPWM_COUNTER_MODE_UP_DOWN);
    
            //
            // Disable phase shifting
            //
            EPWM_disablePhaseShiftLoad(ePWM[j]);
    
            //
            // Set up both EPWM1 clock dividers and disable sync out pulses
            //
            EPWM_setClockPrescaler(ePWM[j],
                                   EPWM_CLOCK_DIVIDER_1,
                                   EPWM_HSCLOCK_DIVIDER_1);
            EPWM_setSyncOutPulseMode(ePWM[j], EPWM_SYNC_OUT_PULSE_DISABLED);
    
            //
            // Set up shadowing
            // MUST BE CTR=(ZER & PRD)
            //
            EPWM_setCounterCompareShadowLoadMode(ePWM[j],
                                                 EPWM_COUNTER_COMPARE_A,
                                                 EPWM_COMP_LOAD_ON_CNTR_ZERO_PERIOD);
            EPWM_setCounterCompareShadowLoadMode(ePWM[j],
                                                 EPWM_COUNTER_COMPARE_B,
                                                 EPWM_COMP_LOAD_ON_CNTR_ZERO_PERIOD);
    
            //
            // Set up Action Qualifiers for Channels A and B
            // (set high on CMPxU, set low on CMPxD for both channels)
            //
    
            EPWM_setActionQualifierAction(ePWM[j],
                                          EPWM_AQ_OUTPUT_A,
                                          EPWM_AQ_OUTPUT_HIGH,
                                          EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
            EPWM_setActionQualifierAction(ePWM[j],
                                          EPWM_AQ_OUTPUT_A,
                                          EPWM_AQ_OUTPUT_LOW,
                                          EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA);
            EPWM_setActionQualifierAction(ePWM[j],
                                          EPWM_AQ_OUTPUT_B,
                                          EPWM_AQ_OUTPUT_HIGH,
                                          EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB);
            EPWM_setActionQualifierAction(ePWM[j],
                                          EPWM_AQ_OUTPUT_B,
                                          EPWM_AQ_OUTPUT_LOW,
                                          EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPB);
    
            //
            // Select Channel A and B control mode to utilize CMPxHR or TBPRDHR
            //
            HRPWM_setMEPControlMode(ePWM[j], HRPWM_CHANNEL_A, HRPWM_MEP_DUTY_PERIOD_CTRL);
            HRPWM_setMEPControlMode(ePWM[j], HRPWM_CHANNEL_B, HRPWM_MEP_DUTY_PERIOD_CTRL);
    
            //
            // Select Channel A and B edge mode to control both edges
            //
            HRPWM_setMEPEdgeSelect(ePWM[j], HRPWM_CHANNEL_A, HRPWM_MEP_CTRL_RISING_AND_FALLING_EDGE);
            HRPWM_setMEPEdgeSelect(ePWM[j], HRPWM_CHANNEL_B, HRPWM_MEP_CTRL_RISING_AND_FALLING_EDGE);
    
            //
            // Set up shadow loading for CMPAHR (this MUST be set to shadow load on CTR=(ZER & PRD))
            //
            HRPWM_setCounterCompareShadowLoadEvent(ePWM[j], HRPWM_CHANNEL_A, HRPWM_LOAD_ON_CNTR_ZERO_PERIOD);
            HRPWM_setCounterCompareShadowLoadEvent(ePWM[j], HRPWM_CHANNEL_B, HRPWM_LOAD_ON_CNTR_ZERO_PERIOD);
    
            //
            // Turn on auto-conversion
            //
            HRPWM_enableAutoConversion(ePWM[j]);
    
            //
            // Turn on high-resolution period control in order to let HR duty control occur on BOTH EDGEs.
            //
            HRPWM_enablePeriodControl(ePWM[j]);
            HRPWM_disablePhaseShiftLoad(ePWM[j]);
    
    
            //
            // Set up an empty interrupt where user can fill with whatever is desired
            // Select INT on Time base counter zero event,
            // Enable INT, generate INT on 1st event
            //
            EPWM_setInterruptSource(ePWM[j], EPWM_INT_TBCTR_ZERO);
            EPWM_enableInterrupt(ePWM[j]);
            EPWM_setInterruptEventCount(ePWM[j], 1U);
    
            //
            // Turn on high-resolution period control.
            //
    
            HRPWM_enablePeriodControl(ePWM[j]);
            HRPWM_enablePhaseShiftLoad(ePWM[j]);
    
            EPWM_forceSyncPulse(ePWM[j]);
        }
    
    }
    
    //
    // error - Halt debugger when called
    //
    void error (void)
    {
        ESTOP0;         // Stop here and handle error
    }
    

    Best Regards,

    Allison

  • Hi Allison,

    Thank you for your reply.

    I will share this code with my clients.

    Best Regards,

    Ito

  • Ok sounds good, Ito.

    Best,

    Allison