Part Number: TMS320F28069
Hello, I get this error when I try to erase or program the C28x Flash.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Stefan,
Can you check the status XRSn pin of the device ?
Regards,
Vivek Singh
Hi Vivek,
I measured on the XRS pin with the oscilloscope while the debugger was connected to the device.
Here you can see the wiring diagram and my measured signal.


I measured on the XRS pin even without a debugger attached. The signal is high until I hit the reset button (S1). Then the signal goes to low.
The same thing happened to me a few weeks ago with another device. What could be the reason for the microcontroller to jump into the low-power mode?
Regards,
Stefan Mayer
Do you have watchdog enable in your application which is causing this reset pulse ?
Vivek Singh