Part Number: TMS320F28379D
hello, I'm triggering the CLA unit on the f28379d processor with a 100kHz pwm interrupt. my question is can I write code into the pwm interrupt function on the main processor that we use when triggering CLA? also, in which unit should I clear the pwm interrupt flag AND the PIR flag, is it in the CLA or pwm interrupt function?