Part Number: TMS320F28375S
Other Parts Discussed in Thread: SYSCONFIG
Hello Team,
I am using ccs 12.6.0 with sysconfig 1.19.0. I want to use FreeRTOS in my project. i am new to this controller. can you please help me with how to start with FreeRTOS in TMS320F28375S?
i have launchpad F28379D for use. i started with configuring FreeRTOS in sysconfig but it is giving error as shown below.


then do some changes in my cmd file.

now, i am able to build my project. but i am not able to execute the task while debugging. my code stucks and not going inside the task.

//###########################################################################
//
// Included Files
//
#include "driverlib.h"
#include "board.h"
#include "FreeRTOS.h"
#include "c2000_freertos.h"
#include "FreeRTOSConfig.h"
//
// Globals
//
//
// Function Prototypes
//
void mcu_task1(void* pvParameters);
//
// Main
//
void main(void)
{
//
// Intialize device clock and peripherals
//
Device_init();
//
// Disable pin locks and enable internal pullups.
//
//Device_initGPIO(); //skipped for this example
//
// Initialize PIE and clear PIE registers. Disables CPU interrupts
//
Interrupt_initModule();
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
//
Interrupt_initVectorTable();
//
// Initialize resources
//
Board_init();
//
// Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
//
EINT;
ERTM;
FreeRTOS_init();
for(;;)
{
}
}
void mcu_task1(void* pvParameters)
{
GPIO_togglePin(19);
vTaskDelay(500);
}
//
// End of file
//
any help will be highly appreciated.
thanks and regards.