Part Number: TMS320F28035-EP
I've read the TRM, but I am still not clear on this point.
Here is my setup.
1. If have three SOCs, SOC4,5, and 6 for example, each with a different ADC channel and sampling window, BUT A SINGLE TRIGGER SOURCE.
What happens when the trigger event occurs, assuming that no other conversions are injected or pending ?
Here is what I "believe" that TRM says.
The SOC with the lowest number (highest priority, SOC4) samples and converts first.
When the EOC for SOC4 completes, the SOC with the next highest priority starts next (SOC5, without a new trigger).
When the EOC for SOC5 completes, SOC6 starts (without a new trigger).
Basically, one trigger, multiple conversions.
Is that how it works ?