TIMEOUT Flag of SCIFLT Reg. is becomes 1 after about 5 seconds.
I want to change that time to 2 seconds.
I can't find source code related to that time.
Is there no way?
thanks for your help.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TIMEOUT Flag of SCIFLT Reg. is becomes 1 after about 5 seconds.
I want to change that time to 2 seconds.
I can't find source code related to that time.
Is there no way?
thanks for your help.
Hello,
The amount of time the LIN bus has to be idle for the TIMEOUT flag to set is something that is setup in the LIN peripheral's design. It is set to trigger after around 4 seconds and cannot be configured/changed on the application level. Can you explain a little more about why you are trying to shorten the time? I can discuss with other experts to see if there is another way to trigger an interrupt on this condition (potentially using another peripheral), based on your use case.
Best Regards,
Delaney
The requirement is 2 seconds. Sleep mode must be performed 2 seconds after LIN communication is disconnected.
Hello,
I believe you could use the CLB module to detect when the line is high for 2 seconds, generate a CLB interrupt on this condition, and then the POWERDOWN bit (SCIGCR2.0) could be set in the CLB ISR. I will loop in an CLB expert to comment on this.
Additionally, what SYSCLK frequency are you using?
Best Regards,
Delaney
Hello Chan,
I believe you could use the CLB module to detect when the line is high for 2 seconds, generate a CLB interrupt on this condition, and then the POWERDOWN bit (SCIGCR2.0) could be set in the CLB ISR.
What Delaney stated here is correct, you can route an input signal from a GPIO pin to the CLB and use the counter to count how long it's high (the counters are 32-bit, so this is feasible). From there, you can create a match condition for the counter to generate an interrupt via the High Level Controller (HLC), and within the interrupt you can perform whatever operations are necessary for your application.