Part Number: TMS320F280039C
Hi Team
Customer try to move PFC control logic form C28x to CLA, but they find when put the same C code into .c file and .cla file, the code size is significantly larger in .cla than in .c, which can be found in found in .map file.
I can also test this issue using "cla_ex4_pwm_control" demo, just to add some simple function and click "build".
Questions are:
1. Why there is the difference happen?
2. How to optimize the CLA code to make the code size as small as possible.
Thanks and best regards
Joe
25th April.