Other Parts Discussed in Thread: DRV8300, LAUNCHXL-F280025C
产品编号:TMS320F2800157
Hi,I encountered the following issues in my incremental build project.I hope you can answer it for me
Q1:I built the project in increments from the Motor Control SDK Generic Project and Lab User Guide (spruj26 filename). Now there is a problem with voltage sampling, the voltage offset coefficient is usually around 0.5, while the value of I is greater than 1 (as shown in Figure p1). Launchpadf2800157 Follow the user guide in Figure p2 to connect drv8323rh, connect the 47nF capacitor to C9, C10, and C11, and do the following according to the relevant questions in the forum:
For S2, place (1) the SEL1 (left) switch up, connect GPIO28 and GPIO29 to the BoosterPack connector, then place (1) the SEL2 (right) switch up, GPIO16 and GPIO17 are then output to the virtual COM at the XDS110 debugger port.
For S3, the SEL1 (left) switch is pulled down to pull GPIO24 to logic 0, and the SEL2 (right) switch is pulled up to pull GPIO32 to logic 1 to put the F280025C in wait-to-start mode, reducing the risk of connection issues or previously loaded code execution.
For S4, if the predefined symbol "CMD_CAN_EN" is set in the project properties, and S4 is set to off (on), GPIO32 and GPIO33 will be routed to the CAN transceiver and the J14 CAN interface
For S5, SEL1 (left) switch is placed down to GPIO44/37/43 routing eQEP1 at encoder interface on J12, and SEL2 (right) switch is placed down to GPIO14/25/2/26 routing eQEP2 at Hall sensor interface on J13.
I used the case of f280015x and drv8323rs. Did it make a difference? If it doesn't work, what's the cause of the problem? How can I fix this?
Q2:In the official case of f280015x motor driver, is Flash_lib_HVKIT_3SC compatible with drv8300? If not, which model is appropriate?
Q3:In the official case, external crystals are used by default. Where can I modify it to use internal crystals?
Thank you for any help!