This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am using CCS12.7 + C2000Ware_5_02_00_00 for my F28P55x project. I was able to configure my F28P55x demo board and ran it yesterday.
I did not change anything thereafter, but for some strange reason, when I tried to configure the board with the same project today, it errors out below:
I then clicked "yes" , then it pops up the window below:
Please advise how to resolve this issue so that I can configure the board .
The file is actually at: C:\Users\Xiaoquan\Documents\JX_CCS_git\JX_QS2_CCS127gitRepository\QS2\targetConfigs\TMS320F28P550SJ9.ccxml
Why does CCS look for it at C:\Users\Xiaoquan\Documents\JX_CCS_git\JX_QS2_CCS127\QS2\targetConfigs? There was no such issue and I was able to configure and run on the board yesterday.