Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Hi,
So, I did applied an inbuilt example of FFT named as 2837x_RFFT_ADC_RT.
In which my main focus was to get phase of adc samples.
It is giving some output using phase buffer array "RFFTphaseBuff" but as of now I'm not able to understand what output it is giving.
I'm giving input using function generator a sine wave of 1KHz frequency, 1 Vpp amplitude, offset of 1Vdc and phase of 0 degree.
Since the phase is 0 still the "RFFTphaseBuff" is changing continusly.
why this is happening??
here I'm attaching screenshot of array output. please go through to it and guide me to get the correct phase of adc sample from the example.
Thanking in anticipation.
Vishwas