This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280033: error #10234-D: unresolved symbols remain

Part Number: TMS320F280033
Other Parts Discussed in Thread: TEST2, C2000WARE

Hi. I have tried to include this library files in many different ways, but I am not able to resolve the error. This gets resolved only when I add the physical files inside my project directory. Am I doing something wrong?

The library file I am trying to include here is driverlib.lib.  I have attached the build log for reference.

Fullscreen
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
**** Build of configuration Debug for project DLIB_TEST2 ****
"C:\\ti\\ccs1250\\ccs\\utils\\bin\\gmake" -k -j 16 all -O
Building file: "../main.c"
Invoking: C2000 Compiler
"C:/ti/ccs1250/ccs/tools/compiler/ti-cgt-c2000_22.6.1.LTS/bin/cl2000" -v28 -ml -mt --float_support=fpu32 --tmu_support=tmu0 --vcu_support=vcrc --include_path="C:/ti/ccs1250/ccs/tools/compiler/ti-cgt-c2000_22.6.1.LTS/include" --include_path="C:/ti/c2000/C2000Ware_5_01_00_00/driverlib/f28003x/driverlib" --include_path="C:/CCS/TEST/DLIB_TEST2" --include_path="C:/CCS/TEST/DLIB_TEST2/misc" -g --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=coffabi --preproc_with_compile --preproc_dependency="main.d_raw" "../main.c"
Finished building: "../main.c"
Building target: "DLIB_TEST2.out"
Invoking: C2000 Linker
"C:/ti/ccs1250/ccs/tools/compiler/ti-cgt-c2000_22.6.1.LTS/bin/cl2000" -v28 -ml -mt --float_support=fpu32 --tmu_support=tmu0 --vcu_support=vcrc -g --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=coffabi -z -m"DLIB_TEST2.map" --stack_size=0x200 --warn_sections -i"C:/ti/ccs1250/ccs/tools/compiler/ti-cgt-c2000_22.6.1.LTS/lib" -i"C:/ti/c2000/C2000Ware_5_01_00_00/driverlib/f28003x/driverlib/ccs/Debug" -i"C:/ti/ccs1250/ccs/tools/compiler/ti-cgt-c2000_22.6.1.LTS/include" --reread_libs --diag_wrap=off --display_error_number --xml_link_info="DLIB_TEST2_linkInfo.xml" --rom_model -o "DLIB_TEST2.out" "./main.obj" "../F280033_flash_lnk.cmd" "C:/ti/c2000/C2000Ware_5_01_00_00/driverlib/f28003x/driverlib/ccs/Debug/driverlib.lib" -llibc.a -l"C:/ti/c2000/C2000Ware_5_01_00_00/driverlib/f28003x/driverlib/ccs/Debug/driverlib.lib" -ldriverlib.lib -l"C:/ti/c2000/C2000Ware_5_01_00_00/driverlib/f28003x/driverlib/ccs/Debug/driverlib.lib"
<Linking>
warning #10373-D: library "C:/ti/c2000/C2000Ware_5_01_00_00/driverlib/f28003x/driverlib/ccs/Debug/driverlib.lib" contains ELF object files which are incompatible with the TI-COFF output file. Ensure you are using the proper library.
warning #10373-D: library "C:/ti/c2000/C2000Ware_5_01_00_00/driverlib/f28003x/driverlib/ccs/Debug/driverlib.lib" contains ELF object files which are incompatible with the TI-COFF output file. Ensure you are using the proper library.
warning #10373-D: library "C:/ti/c2000/C2000Ware_5_01_00_00/driverlib/f28003x/driverlib/ccs/Debug/driverlib.lib" contains ELF object files which are incompatible with the TI-COFF output file. Ensure you are using the proper library.
warning #10373-D: library "C:/ti/c2000/C2000Ware_5_01_00_00/driverlib/f28003x/driverlib/ccs/Debug/driverlib.lib" contains ELF object files which are incompatible with the TI-COFF output file. Ensure you are using the proper library.
warning #10373-D: library "C:/ti/c2000/C2000Ware_5_01_00_00/driverlib/f28003x/driverlib/ccs/Debug/driverlib.lib" contains ELF object files which are incompatible with the TI-COFF output file. Ensure you are using the proper library.
warning #10373-D: library "C:/ti/c2000/C2000Ware_5_01_00_00/driverlib/f28003x/driverlib/ccs/Debug/driverlib.lib" contains ELF object files which are incompatible with the TI-COFF output file. Ensure you are using the proper library.
warning #10373-D: library "C:/ti/c2000/C2000Ware_5_01_00_00/driverlib/f28003x/driverlib/ccs/Debug/driverlib.lib" contains ELF object files which are incompatible with the TI-COFF output file. Ensure you are using the proper library.
warning #10373-D: library "C:/ti/c2000/C2000Ware_5_01_00_00/driverlib/f28003x/driverlib/ccs/Debug/driverlib.lib" contains ELF object files which are incompatible with the TI-COFF output file. Ensure you are using the proper library.
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX