This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
We used this product under the environment of 25° temperature, 40RH humidity, and 3.3V voltage. The specific situation is as follows: The burner self-test failed and the chip could not be burned.
Burner function, using J-TAG interface burning, as shown below:
Could you please help us to confirm the cause and how should we solve this anomaly
Thank you
Hi our subject matter expert is out of the office today but should be able to respond later this week. In the meantime, can you please answer the following questions:
1) What C2000 device are you programming?
2) Have you ever successfully programmed this C2000 device with C2000-GANG?
3) If yes, how many devices have been successful? How many are failing?
1) The chip model of the test is TMS320F280049 2) The only board of this product in hand 3) The test has failed for many times
I apologize, the SME had to extend his absence and wont return until Tuesday. In the meantime, let me ask a few questions:
I presume this is a custom board and not TI hardware, please correct me if wrong.
1) Is it a new design or has it been in production?
2) Are you able to program the device with a JTAG debug probe (e.g. XDS110) and CCS/Uniflash without the C2000-GANG?
3) Is this the first time you are using C2000-GANG or have you successfully used it on any project?
Also, can you reply what error message the C2000-GANG is giving you as well as the FW revision on the C2000-GANG SW.
Best,
Matthew
Hi
We are the first time to use the C2000 burner, there is no XDS110 burner, we have not done the C2000 series MCU products before
We have not purchased the XDS110. The attachment is the specific bad conditions we burned, please help to confirm
thank you
=== C2000-GANG Self test results ( Monday, April 29, 2024, 10:48:37 ) === Adapter SN ------: 23010179 Hardware --------: C2K : 01.06 Access key ------: C2000 - Gang Programmer Silicon Number --: D3D7 986E 1700 2800 API Firmware ----: C2K-Gang AC28: 01.00.04.06 BOOT Firmware ---: G430BOOT B430: 01.00.02.00 GUI Software ----: C2000-Gang-GUI G28x: 01.00.04.06 DLL Software ----: C2000-Gang-DLL D280: 01.00.04.06 ================ Test results ============= No. name parameter limits result status 1: Data Bus (ALL LOW) 0x0000 (0x0000 - 0x0000) Result: 0x00 ... >> OK << 2: Data Bus (ALL HIGH) 0x00FF (0xFFFF - 0xFFFF) Result: 0xFFFF ... >> OK << 3: Data Bus (D-0 HI ) 0x0001 (0x0101 - 0x0101) Result: 0x0101 ... >> OK << 4: Data Bus (D-1 HI ) 0x0002 (0x0202 - 0x0202) Result: 0x0202 ... >> OK << 5: Data Bus (D-2 HI ) 0x0004 (0x0404 - 0x0404) Result: 0x0404 ... >> OK << 6: Data Bus (D-3 HI ) 0x0008 (0x0808 - 0x0808) Result: 0x0808 ... >> OK << 7: Data Bus (D-4 HI ) 0x0010 (0x1010 - 0x1010) Result: 0x1010 ... >> OK << 8: Data Bus (D-5 HI ) 0x0020 (0x2020 - 0x2020) Result: 0x2020 ... >> OK << 9: Data Bus (D-6 HI ) 0x0040 (0x4040 - 0x4040) Result: 0x4040 ... >> OK << 10: Data Bus (D-7 HI ) 0x0080 (0x8080 - 0x8080) Result: 0x8080 ... >> OK << 11: Data-2 Bus (ALL LOW) 0x0000 (0x0000 - 0x0000) Result: 0x00 ... >> OK << 12: Data-2 Bus (ALL HIGH) 0x00FF (0xFFFF - 0xFFFF) Result: 0xFFFF ... >> OK << 13: Data-2 Bus (D2-0 HI ) 0x0001 (0x0101 - 0x0101) Result: 0x0101 ... >> OK << 14: Data-2 Bus (D2-1 HI ) 0x0002 (0x0202 - 0x0202) Result: 0x0202 ... >> OK << 15: Data-2 Bus (D2-2 HI ) 0x0004 (0x0404 - 0x0404) Result: 0x0404 ... >> OK << 16: Data-2 Bus (D2-3 HI ) 0x0008 (0x0808 - 0x0808) Result: 0x0808 ... >> OK << 17: Data-2 Bus (D2-4 HI ) 0x0010 (0x1010 - 0x1010) Result: 0x1010 ... >> OK << 18: Data-2 Bus (D2-5 HI ) 0x0020 (0x2020 - 0x2020) Result: 0x2020 ... >> OK << 19: Data-2 Bus (D2-6 HI ) 0x0040 (0x4040 - 0x4040) Result: 0x4040 ... >> OK << 20: Data-2 Bus (D2-7 HI ) 0x0080 (0x8080 - 0x8080) Result: 0x8080 ... >> OK << 21: Vcc Target-1 (ALL OFF) 0.00 V ( 0.00 to 0.30) Result: 0.02 V ... >> OK << 22: Vcc Target-2 (ALL OFF) 0.00 V ( 0.00 to 0.30) Result: 0.01 V ... >> OK << 23: Vcc Target-3 (ALL OFF) 0.00 V ( 0.00 to 0.30) Result: 0.01 V ... >> OK << 24: Vcc Target-4 (ALL OFF) 0.00 V ( 0.00 to 0.30) Result: 0.01 V ... >> OK << 25: Vcc Target-5 (ALL OFF) 0.00 V ( 0.00 to 0.30) Result: 0.01 V ... >> OK << 26: Vcc Target-6 (ALL OFF) 0.00 V ( 0.00 to 0.30) Result: 0.01 V ... >> OK << 27: Vcc Target-7 (ALL OFF) 0.00 V ( 0.00 to 0.30) Result: 0.01 V ... >> OK << 28: Vcc Target-8 (ALL OFF) 0.00 V ( 0.00 to 0.30) Result: 0.01 V ... >> OK << 29: Translators VT (OFF) 0.00 V ( 0.00 to 0.50) Result: 0.02 V ... >> OK << 30: Translators VT (ON 3.3V) 3.30 V ( 3.10 to 3.50) Result: 3.17 V ... >> OK << 31: Vpp Voltage-in 10.00 V ( 8.00 to 12.00) Result: 10.42 V ... >> OK << 32: Vpp Voltage 7.00 V ( 6.50 to 7.30) Result: 6.88 V ... >> OK << 33: Internal Vcc-3.3V 3.30 V ( 3.20 to 3.40) Result: 3.30 V ... >> OK << 34: Vcc Target-1 (ALL ON 3.3V) 3.30 V ( 3.10 to 3.50) Result: 0.15 V ... >> ERROR << 35: Vcc Target-2 (ALL ON 3.3V) 3.30 V ( 3.10 to 3.50) Result: 0.14 V ... >> ERROR << 36: Vcc Target-3 (ALL ON 3.3V) 3.30 V ( 3.10 to 3.50) Result: 0.14 V ... >> ERROR << 37: Vcc Target-4 (ALL ON 3.3V) 3.30 V ( 3.10 to 3.50) Result: 0.14 V ... >> ERROR << 38: Vcc Target-5 (ALL ON 3.3V) 3.30 V ( 3.10 to 3.50) Result: 0.14 V ... >> ERROR << 39: Vcc Target-6 (ALL ON 3.3V) 3.30 V ( 3.10 to 3.50) Result: 0.14 V ... >> ERROR << 40: Vcc Target-7 (ALL ON 3.3V) 3.30 V ( 3.10 to 3.50) Result: 0.14 V ... >> ERROR << 41: Vcc Target-8 (ALL ON 3.3V) 3.30 V ( 3.10 to 3.50) Result: 0.14 V ... >> ERROR << 42: Vcc discharge (50ms)Target-1 3.30 V ( 0.30 to 1.50) Result: 0.20 V ... >> ERROR << 43: Vcc discharge (50ms)Target-2 3.30 V ( 0.30 to 1.50) Result: 0.20 V ... >> ERROR << 44: Vcc discharge (50ms)Target-3 3.30 V ( 0.30 to 1.50) Result: 0.19 V ... >> ERROR << 45: Vcc discharge (50ms)Target-4 3.30 V ( 0.30 to 1.50) Result: 0.19 V ... >> ERROR << 46: Vcc discharge (50ms)Target-5 3.30 V ( 0.30 to 1.50) Result: 0.19 V ... >> ERROR << 47: Vcc discharge (50ms)Target-6 3.30 V ( 0.30 to 1.50) Result: 0.19 V ... >> ERROR << 48: Vcc discharge (50ms)Target-7 3.30 V ( 0.30 to 1.50) Result: 0.19 V ... >> ERROR << 49: Vcc discharge (50ms)Target-8 3.30 V ( 0.30 to 1.50) Result: 0.19 V ... >> ERROR << 50: Vcc Target-1 ( #1 ON ) 0.00 V ( 3.10 to 3.50) Result: 0.20 V ... >> ERROR << 51: Vcc Target-2 ( #1 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.20 V ... >> OK << 52: Vcc Target-3 ( #1 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 53: Vcc Target-4 ( #1 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 54: Vcc Target-5 ( #1 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 55: Vcc Target-6 ( #1 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 56: Vcc Target-7 ( #1 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 57: Vcc Target-8 ( #1 ON ) 3.30 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 58: Vcc Target-1 ( #2 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.20 V ... >> OK << 59: Vcc Target-2 ( #2 ON ) 0.00 V ( 3.10 to 3.50) Result: 0.20 V ... >> ERROR << 60: Vcc Target-3 ( #2 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 61: Vcc Target-4 ( #2 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 62: Vcc Target-5 ( #2 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 63: Vcc Target-6 ( #2 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 64: Vcc Target-7 ( #2 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 65: Vcc Target-8 ( #2 ON ) 3.30 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 66: Vcc Target-1 ( #3 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.20 V ... >> OK << 67: Vcc Target-2 ( #3 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.20 V ... >> OK << 68: Vcc Target-3 ( #3 ON ) 0.00 V ( 3.10 to 3.50) Result: 0.19 V ... >> ERROR << 69: Vcc Target-4 ( #3 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 70: Vcc Target-5 ( #3 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 71: Vcc Target-6 ( #3 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 72: Vcc Target-7 ( #3 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 73: Vcc Target-8 ( #3 ON ) 3.30 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 74: Vcc Target-1 ( #4 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.20 V ... >> OK << 75: Vcc Target-2 ( #4 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 76: Vcc Target-3 ( #4 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 77: Vcc Target-4 ( #4 ON ) 0.00 V ( 3.10 to 3.50) Result: 0.19 V ... >> ERROR << 78: Vcc Target-5 ( #4 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 79: Vcc Target-6 ( #4 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 80: Vcc Target-7 ( #4 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 81: Vcc Target-8 ( #4 ON ) 3.30 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 82: Vcc Target-1 ( #5 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.20 V ... >> OK << 83: Vcc Target-2 ( #5 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 84: Vcc Target-3 ( #5 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 85: Vcc Target-4 ( #5 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 86: Vcc Target-5 ( #5 ON ) 0.00 V ( 3.10 to 3.50) Result: 0.19 V ... >> ERROR << 87: Vcc Target-6 ( #5 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 88: Vcc Target-7 ( #5 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 89: Vcc Target-8 ( #5 ON ) 3.30 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 90: Vcc Target-1 ( #6 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.20 V ... >> OK << 91: Vcc Target-2 ( #6 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.20 V ... >> OK << 92: Vcc Target-3 ( #6 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 93: Vcc Target-4 ( #6 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 94: Vcc Target-5 ( #6 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 95: Vcc Target-6 ( #6 ON ) 0.00 V ( 3.10 to 3.50) Result: 0.19 V ... >> ERROR << 96: Vcc Target-7 ( #6 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 97: Vcc Target-8 ( #6 ON ) 3.30 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 98: Vcc Target-1 ( #7 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.20 V ... >> OK << 99: Vcc Target-2 ( #7 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 100: Vcc Target-3 ( #7 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 101: Vcc Target-4 ( #7 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 102: Vcc Target-5 ( #7 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 103: Vcc Target-6 ( #7 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 104: Vcc Target-7 ( #7 ON ) 0.00 V ( 3.10 to 3.50) Result: 0.19 V ... >> ERROR << 105: Vcc Target-8 ( #7 ON ) 3.30 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 106: Vcc Target-1 ( #8 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.20 V ... >> OK << 107: Vcc Target-2 ( #8 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 108: Vcc Target-3 ( #8 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 109: Vcc Target-4 ( #8 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 110: Vcc Target-5 ( #8 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 111: Vcc Target-6 ( #8 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 112: Vcc Target-7 ( #8 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.19 V ... >> OK << 113: Vcc Target-8 ( #8 ON ) 3.30 V ( 3.10 to 3.50) Result: 0.19 V ... >> ERROR << 114: SD Power OFF 0x0000 (0x0000 - 0x0000) Result: 0x00 ... >> OK << 115: SD Power ON 0x0001 (0x0001 - 0x0001) Result: 0x01 ... >> OK << 116: SD Discharge - delay 2ms 0x0010 (0x0001 - 0x0001) Result: 0x01 ... >> OK << 117: SD Discharge - delay 50ms 0x0010 (0x0000 - 0x0000) Result: 0x00 ... >> OK << 118: BSL RX bus (#1 HIGH) 0x0001 (0x0001 - 0x0001) Result: 0x01 ... >> OK << 119: BSL RX bus (#2 HIGH) 0x0002 (0x0002 - 0x0002) Result: 0x02 ... >> OK << 120: BSL RX bus (#3 HIGH) 0x0004 (0x0004 - 0x0004) Result: 0x04 ... >> OK << 121: BSL RX bus (#4 HIGH) 0x0008 (0x0008 - 0x0008) Result: 0x08 ... >> OK << 122: BSL RX bus (#5 HIGH) 0x0010 (0x0010 - 0x0010) Result: 0x10 ... >> OK << 123: BSL RX bus (#6 HIGH) 0x0020 (0x0020 - 0x0020) Result: 0x20 ... >> OK << 124: BSL RX bus (#7 HIGH) 0x0040 (0x0040 - 0x0040) Result: 0x40 ... >> OK << 125: BSL RX bus (#8 HIGH) 0x0080 (0x0080 - 0x0080) Result: 0x80 ... >> OK << 126: BSL TX bus (#1 HIGH) 0x0001 (0x0001 - 0x0001) Result: 0x01 ... >> OK << 127: BSL TX bus (#2 HIGH) 0x0002 (0x0002 - 0x0002) Result: 0x02 ... >> OK << 128: BSL TX bus (#3 HIGH) 0x0004 (0x0004 - 0x0004) Result: 0x04 ... >> OK << 129: BSL TX bus (#4 HIGH) 0x0008 (0x0008 - 0x0008) Result: 0x08 ... >> OK << 130: BSL TX bus (#5 HIGH) 0x0010 (0x0010 - 0x0010) Result: 0x10 ... >> OK << 131: BSL TX bus (#6 HIGH) 0x0020 (0x0020 - 0x0020) Result: 0x20 ... >> OK << 132: BSL TX bus (#7 HIGH) 0x0040 (0x0040 - 0x0040) Result: 0x40 ... >> OK << 133: BSL TX bus (#8 HIGH) 0x0080 (0x0080 - 0x0080) Result: 0x80 ... >> OK << 134: TDI bus (#8 HIGH) 0x0080 (0x0080 - 0x0080) Result: 0x80 ... >> OK << 135: TDI bus (#1 HIGH) 0x0001 (0x0001 - 0x0001) Result: 0x01 ... >> OK << 136: TDI bus (#2 HIGH) 0x0002 (0x0002 - 0x0002) Result: 0x02 ... >> OK << 137: TDI bus (#3 HIGH) 0x0004 (0x0004 - 0x0004) Result: 0x04 ... >> OK << 138: TDI bus (#4 HIGH) 0x0008 (0x0008 - 0x0008) Result: 0x08 ... >> OK << 139: TDI bus (#5 HIGH) 0x0010 (0x0010 - 0x0010) Result: 0x10 ... >> OK << 140: TDI bus (#6 HIGH) 0x0020 (0x0020 - 0x0020) Result: 0x20 ... >> OK << 141: TDI bus (#7 HIGH) 0x0040 (0x0040 - 0x0040) Result: 0x40 ... >> OK << 142: TDIO Tx-bus (#1 HIGH) 0x0001 (0x0001 - 0x0001) Result: 0x01 ... >> OK << 143: TDIO Tx-bus (#2 HIGH) 0x0002 (0x0002 - 0x0002) Result: 0x02 ... >> OK << 144: TDIO Tx-bus (#3 HIGH) 0x0004 (0x0004 - 0x0004) Result: 0x04 ... >> OK << 145: TDIO Tx-bus (#4 HIGH) 0x0008 (0x0008 - 0x0008) Result: 0x08 ... >> OK << 146: TDIO Tx-bus (#5 HIGH) 0x0010 (0x0010 - 0x0010) Result: 0x10 ... >> OK << 147: TDIO Tx-bus (#6 HIGH) 0x0020 (0x0020 - 0x0020) Result: 0x20 ... >> OK << 148: TDIO Tx-bus (#7 HIGH) 0x0040 (0x0040 - 0x0040) Result: 0x40 ... >> OK << 149: TDIO Tx-bus (#8 HIGH) 0x0080 (0x0080 - 0x0080) Result: 0x80 ... >> OK << 150: TDIO Tx-Rx (#1 HIGH) 0x0001 (0x0001 - 0x0001) Result: 0x01 ... >> OK << 151: TDIO Tx-Rx (#2 HIGH) 0x0002 (0x0002 - 0x0002) Result: 0x02 ... >> OK << 152: TDIO Tx-Rx (#3 HIGH) 0x0004 (0x0004 - 0x0004) Result: 0x04 ... >> OK << 153: TDIO Tx-Rx (#4 HIGH) 0x0008 (0x0008 - 0x0008) Result: 0x08 ... >> OK << 154: TDIO Tx-Rx (#5 HIGH) 0x0010 (0x0010 - 0x0010) Result: 0x10 ... >> OK << 155: TDIO Tx-Rx (#6 HIGH) 0x0020 (0x0020 - 0x0020) Result: 0x20 ... >> OK << 156: TDIO Tx-Rx (#7 HIGH) 0x0040 (0x0040 - 0x0040) Result: 0x40 ... >> OK << 157: TDIO Tx-Rx (#8 HIGH) 0x0080 (0x0080 - 0x0080) Result: 0x80 ... >> OK << 158: TDIO Rx-bus (#1 HIGH) 0x0001 (0x0001 - 0x0001) Result: 0x01 ... >> OK << 159: TDIO Rx-bus (#2 HIGH) 0x0002 (0x0002 - 0x0002) Result: 0x02 ... >> OK << 160: TDIO Rx-bus (#3 HIGH) 0x0004 (0x0004 - 0x0004) Result: 0x04 ... >> OK << 161: TDIO Rx-bus (#4 HIGH) 0x0008 (0x0008 - 0x0008) Result: 0x08 ... >> OK << 162: TDIO Rx-bus (#5 HIGH) 0x0010 (0x0010 - 0x0010) Result: 0x10 ... >> OK << 163: TDIO Rx-bus (#6 HIGH) 0x0020 (0x0020 - 0x0020) Result: 0x20 ... >> OK << 164: TDIO Rx-bus (#7 HIGH) 0x0040 (0x0040 - 0x0040) Result: 0x40 ... >> OK << 165: TDIO Rx-bus (#84 HIGH) 0x0080 (0x0080 - 0x0080) Result: 0x80 ... >> OK << 166: TMS bus (All HIGH) 0x00FF (0x00FF - 0x00FF) Result: 0xFF ... >> OK << 167: TMS bus (All LOW) 0x0000 (0x0000 - 0x0000) Result: 0x00 ... >> OK << 168: TMS bus (#1 HIGH) 0x0001 (0x0001 - 0x0001) Result: 0x01 ... >> OK << 169: TMS bus (#2 HIGH) 0x0002 (0x0002 - 0x0002) Result: 0x02 ... >> OK << 170: TMS bus (#3 HIGH) 0x0004 (0x0004 - 0x0004) Result: 0x04 ... >> OK << 171: TMS bus (#4 HIGH) 0x0008 (0x0008 - 0x0008) Result: 0x08 ... >> OK << 172: TMS bus (#5 HIGH) 0x0010 (0x0010 - 0x0010) Result: 0x10 ... >> OK << 173: TMS bus (#6 HIGH) 0x0020 (0x0020 - 0x0020) Result: 0x20 ... >> OK << 174: TMS bus (#7 HIGH) 0x0040 (0x0040 - 0x0040) Result: 0x40 ... >> OK << 175: TMS bus (#8 HIGH) 0x0080 (0x0080 - 0x0080) Result: 0x80 ... >> OK << 176: RST bus (All HIGH) 0x00FF (0x00FF - 0x00FF) Result: 0xFF ... >> OK << 177: RST bus (All LOW) 0x0000 (0x0000 - 0x0000) Result: 0x00 ... >> OK << 178: RST bus (#1 HIGH) 0x0001 (0x0001 - 0x0001) Result: 0x01 ... >> OK << 179: RST bus (#2 HIGH) 0x0002 (0x0002 - 0x0002) Result: 0x02 ... >> OK << 180: RST bus (#3 HIGH) 0x0004 (0x0004 - 0x0004) Result: 0x04 ... >> OK << 181: RST bus (#4 HIGH) 0x0008 (0x0008 - 0x0008) Result: 0x08 ... >> OK << 182: RST bus (#5 HIGH) 0x0010 (0x0010 - 0x0010) Result: 0x10 ... >> OK << 183: RST bus (#6 HIGH) 0x0020 (0x0020 - 0x0020) Result: 0x20 ... >> OK << 184: RST bus (#7 HIGH) 0x0040 (0x0040 - 0x0040) Result: 0x40 ... >> OK << 185: RST bus (#8 HIGH) 0x0080 (0x0080 - 0x0080) Result: 0x80 ... >> OK << 186: Keys buffer (All pull-up) 0x001F (0x001F - 0x001F) Result: 0x1F ... >> OK << 187: Access to LCD RAM (0xAA) 0x00AA (0x00AA - 0x00AA) Result: 0xAA ... >> OK << 188: Access to LCD RAM (0x99) 0x0099 (0x0099 - 0x0099) Result: 0x99 ... >> OK << 189: Image Flash Access (get ID) 0x0002 (0x0001 - 0x0002) Result: 0x00 ... >> ERROR << 190: TDI Fuse keys (#1 ON) 0x0001 (0x0001 - 0x0001) Result: 0x01 ... >> OK << 191: TDI Fuse keys (#2 ON) 0x0002 (0x0002 - 0x0002) Result: 0x02 ... >> OK << 192: TDI Fuse keys (#3 ON) 0x0004 (0x0004 - 0x0004) Result: 0x04 ... >> OK << 193: TDI Fuse keys (#4 ON) 0x0008 (0x0008 - 0x0008) Result: 0x08 ... >> OK << 194: TDI Fuse keys (#5 ON) 0x0010 (0x0010 - 0x0010) Result: 0x10 ... >> OK << 195: TDI Fuse keys (#6 ON) 0x0020 (0x0020 - 0x0020) Result: 0x20 ... >> OK << 196: TDI Fuse keys (#7 ON) 0x0040 (0x0040 - 0x0040) Result: 0x40 ... >> OK << 197: TDI Fuse keys (#8 ON) 0x0080 (0x0080 - 0x0080) Result: 0x80 ... >> OK << 198: TEST Fuse keys (#1 ON) 1.00 ( 2.80 to 3.50) Result: 0.00 ... >> ERROR << 199: TEST Fuse keys (#2 ON) 2.00 ( 2.80 to 3.50) Result: 0.00 ... >> ERROR << 200: TEST Fuse keys (#3 ON) 3.00 ( 2.80 to 3.50) Result: 0.00 ... >> ERROR << 201: TEST Fuse keys (#4 ON) 4.00 ( 2.80 to 3.50) Result: 0.00 ... >> ERROR << 202: TEST Fuse keys (#5 ON) 5.00 ( 2.80 to 3.50) Result: 0.00 ... >> ERROR << 203: TEST Fuse keys (#6 ON) 6.00 ( 2.80 to 3.50) Result: 0.00 ... >> ERROR << 204: TEST Fuse keys (#7 ON) 7.00 ( 2.80 to 3.50) Result: 0.00 ... >> ERROR << 205: TEST Fuse keys (#8 ON) 8.00 ( 2.80 to 3.50) Result: 0.00 ... >> ERROR << ============== Finished ================================= * Test failed!! 33 error(s). =========================================================
Thank you for the test log. This looks to be failing for not detecting power to the device(C2000). Pin 5 of the JTAG header should be shorted to the VDDIO(3.3V) supply of the C2000/PCB; the debugger checks the voltage on this pin to verify that the device is powered before attempting the connection.
Can you verify on your PCB that pin5 has a voltage during the test? This pin is usually called "PD" for power detect, I'm not certain why it is listed as Vext on your schematic.
Best,
Matthew