This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am developing the C# program to control C2000 Gang Programmer using DLL with example provided. I have issue to with the InteractiveProcess(INT32 lTime) syntax, it not response and make the device hang. What do I suppose to set before I can use this function and my intention is to make it functioning like the C2000 Gang Programmer GUI in Interactive mode that use file in the PC to Flash not from the Image Memory.
Another problem that I face is to use the GetProgressStatus(void* lPdata). Can you show some example for me?
Regards
Hafiidz
Hi Hafiidz,
Thank you for using our tools. Please download the latest software for MSP-GANG
and you will find examples with interactive mode (in Cpp, but you can do it in sililar way in C#). The software structure is the same as in the C2000-GANG. Above example would be useful.
BTW – I assume that with the image mode you are using you are not reloading image every time, but just once for particular application. You can reprogram image memory 10000 times and after that the image can be corrupted.
Best regards,
Gregory Czajkowski
Elprotronic Inc.