Part Number: TMS320F28379D
Other Parts Discussed in Thread: LAUNCHXL-F28379D, C2000WARE, SYSCONFIG
Tool/software:
Hello,
I am looking for help with flashing the ipc_ex2_gpio_sysconfig example from Resource Explorer (C2000Ware - 5.02.00.00/English/Devices/F2837XD/F28379D/Examples/Driverlib/dual/ipc/) on LAUNCHXL-F28379D. The build configuration is set to FLASH. When I flash the program in the debug state (and start each core at a time) the program works as expected. The LEDs continue flashing even after I stop the debug process. However, when I flash the code into the flash to run as a standalone, the program never operates (i.e. the LEDs never blink). Is there something in sysconfig file that needs to be changed to be able to run the code as soon as the LaunchPad is powered?
Thank you.
Regards,
Leon