Part Number: LAUNCHXL-F28379D
Tool/software:
Hello, I took a look at the adc continuous dma example. It was configured to only do one adc transfer, then the program ends. I made some modifications to the program so that when the DMA ends it begins a new ADC DMA. This all works perfectly however when I specify a set sample amount (64) for a waveform that is 60Hz, I get discontinuities on the edge of each DMA cycle. I tried adjusting the EPWM module to have a frequency that matches the scenario but changing the EPWM count did not appear to do anything. Does anyone know how I can configure this so it has consistent timing?
//###########################################################################
//
// FILE: adc_ex6_soc_continuous_dma.c
//
// TITLE: ADC continuous conversions read by DMA.
//
//! \addtogroup driver_example_list
//! <h1> ADC Continuous Conversions Read by DMA (adc_soc_continuous_dma)</h1>
//!
//! This example sets up two ADC channels to convert simultaneously. The
//! results will be transferred by the DMA into a buffer in RAM.
//!
//! \b External \b Connections \n
//! - A3 & D3 pins should be connected to signals to convert
//!
//! \b Watch \b Variables \n
//! - \b adcADataBuffer \b: a digital representation of the voltage on pin A3\n
//! - \b adcDDataBuffer \b: a digital representation of the voltage on pin D3\n
//!
//
//#############################################################################
//
//
// $Copyright:
// Copyright (C) 2013-2024 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//#############################################################################
//
// Included Files
#include "driverlib.h"
#include "device.h"
// Function Prototypes
__interrupt void adcA1ISR(void);
__interrupt void dmach1ISR(void);
void configureEPWM(uint32_t epwmBase);
void configureADC(uint32_t adcBase);
void Continuous(uint32_t adcBase, uint16_t channel);
void setupADCContinuous(uint32_t adcBase, uint16_t channel);
void initializeDMA(void);
void configureDMAChannels(void);
// Defines
#define RESULTS_BUFFER_SIZE 64 //buffer for storing conversion results
#define EX_ADC_RESOLUTION 16
// 12 for 12-bit conversion resolution, which supports (ADC_MODE_SINGLE_ENDED)
// Sample on single pin (VREFLO is the low reference)
// Or 16 for 16-bit conversion resolution, which supports (ADC_MODE_DIFFERENTIAL)
// Sample on pair of pins (difference between pins is converted, subject to
// common mode voltage requirements; see the device data manual)
// Globals
#pragma DATA_SECTION(adcADataBuffer, "ramgs0");
uint16_t adcADataBuffer[RESULTS_BUFFER_SIZE];
volatile uint16_t done;
void main(void)
{
uint16_t resultsIndex;
// Initialize device clock and peripherals
Device_init();
// Disable pin locks and enable internal pullups.
Device_initGPIO();
// Initialize PIE and clear PIE registers. Disables CPU interrupts.
Interrupt_initModule();
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
Interrupt_initVectorTable();
// Set up ISRs used by this example
// ISR for ADCA INT1 - occurs after first conversion
// ISR for DMA ch1 - occurs when DMA transfer is complete
Interrupt_register(INT_ADCA1, &adcA1ISR);
Interrupt_register(INT_DMA_CH1, &dmach1ISR);
// Enable specific PIE & CPU interrupts:
// ADCA INT1 - Group 1, interrupt 1
// DMA interrupt - Group 7, interrupt 1
Interrupt_enable(INT_ADCA1);
Interrupt_enable(INT_DMA_CH1);
// Stop the ePWM clock
SysCtl_disablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
// Call the set up function for ePWM 2
configureEPWM(EPWM2_BASE);
// Start the ePWM clock
SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
// Configure the ADCA & ADCD and power it up
configureADC(ADCA_BASE);
// Setup the ADC for continuous conversions on channels A3 and D3
setupADCContinuous(ADCA_BASE, 3);
// Initialize the DMA & configure DMA channels 1 & 2
initializeDMA();
configureDMAChannels();
// Initialize results buffer
for(resultsIndex = 0; resultsIndex < RESULTS_BUFFER_SIZE; resultsIndex++)
{
adcADataBuffer[resultsIndex] = 0;
}
// Clearing all pending interrupt flags
DMA_clearTriggerFlag(DMA_CH1_BASE); // DMA channel 1
HWREGH(ADCA_BASE + ADC_O_INTFLGCLR) = 0x3U; // ADCA
EPWM_forceADCTriggerEventCountInit(EPWM2_BASE, EPWM_SOC_A); // EPWM2 SOCA
EPWM_clearADCTriggerFlag(EPWM2_BASE, EPWM_SOC_A); // EPWM2 SOCA
// Enable continuous operation by setting the last SOC to re-trigger
// the first
ADC_setInterruptSOCTrigger(ADCA_BASE, ADC_SOC_NUMBER0, // ADCA
ADC_INT_SOC_TRIGGER_ADCINT2);
// Enable global Interrupts and higher priority real-time debug events:
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
// Start DMA
done = 0;
DMA_startChannel(DMA_CH1_BASE);
// Finally, enable the SOCA trigger from ePWM. This will kick off
// conversions at the next ePWM event.
EPWM_enableADCTrigger(EPWM2_BASE, EPWM_SOC_A);
// Loop until the ISR signals the transfer is complete
while(done == 0)
{
__asm(" NOP");
}
}
// adcA1ISR - This is called after the very first conversion and will disable
// the ePWM SOC to avoid re-triggering problems.
#pragma CODE_SECTION(adcA1ISR, ".TI.ramfunc");
__interrupt void adcA1ISR(void)
{
// Remove ePWM trigger
EPWM_disableADCTrigger(EPWM2_BASE, EPWM_SOC_A);
// Disable this interrupt from happening again
Interrupt_disable(INT_ADCA1);
// Acknowledge interrupt of ADC and DMA
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP7);
}
// dmach1ISR - This is called at the end of the DMA transfer, the conversions
// are stopped by removing the trigger of the first SOC from
// the last.
#pragma CODE_SECTION(dmach1ISR, ".TI.ramfunc");
__interrupt void dmach1ISR(void)
{
// Clear the DMA interrupt flag
DMA_clearTriggerFlag(DMA_CH1_BASE);
// Acknowledge interrupt
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP7);
}
// configureEPWM - Set up the ePWM2 module so that the A output has a period
// of 40us with a 50% duty. The SOCA signal is coincident with
// the rising edge of this.
void configureEPWM(uint32_t epwmBase)
{
// Make the timer count up with a period of
HWREGH(epwmBase + EPWM_O_TBCTL) = 0x0000U;
EPWM_setTimeBasePeriod(epwmBase, 26040U);
// Set the A output on zero and reset on CMPA
EPWM_setActionQualifierAction(epwmBase, EPWM_AQ_OUTPUT_A,
EPWM_AQ_OUTPUT_HIGH,
EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO);
EPWM_setActionQualifierAction(epwmBase, EPWM_AQ_OUTPUT_A,
EPWM_AQ_OUTPUT_LOW,
EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
// Set CMPA to 130.21us to get a 50% duty
EPWM_setCounterCompareValue(epwmBase, EPWM_COUNTER_COMPARE_A, 13020U);
// Start ADC when timer equals zero (note: don't enable yet)
EPWM_setADCTriggerSource(epwmBase, EPWM_SOC_A, EPWM_SOC_TBCTR_ZERO);
EPWM_setADCTriggerEventPrescale(epwmBase, EPWM_SOC_A, 1U);
}
// configureADC - Write ADC configurations and power up the ADC
void configureADC(uint32_t adcBase)
{
// Set ADCDLK divider to /4
ADC_setPrescaler(adcBase, ADC_CLK_DIV_4_0);
// Set resolution and signal mode (see #defines above) and load
// corresponding trims.
#if(EX_ADC_RESOLUTION == 12)
ADC_setMode(adcBase, ADC_RESOLUTION_12BIT, ADC_MODE_SINGLE_ENDED);
#elif(EX_ADC_RESOLUTION == 16)
ADC_setMode(adcBase, ADC_RESOLUTION_16BIT, ADC_MODE_DIFFERENTIAL);
#endif
//
// Set pulse positions to late
//
ADC_setInterruptPulseMode(adcBase, ADC_PULSE_END_OF_CONV);
//
// Power up the ADCs and then delay for 1 ms
//
ADC_enableConverter(adcBase);
//
// Delay for 1ms to allow ADC time to power up
//
DEVICE_DELAY_US(1000);
}
//
// setupADCContinuous - setup the ADC to continuously convert on one channel
//
void setupADCContinuous(uint32_t adcBase, uint16_t channel)
{
uint16_t acqps;
//
// Determine minimum acquisition window (in SYSCLKS) based on resolution
//
if(EX_ADC_RESOLUTION == 12)
{
acqps = 14; // 75ns
}
else //resolution is 16-bit
{
acqps = 63; // 320ns
}
acqps = 8;
//
// Configure SOCs channel no. & acquisition window.
// Trigger SCO0 from EPWM2SOCA.
// Trigger all other SOCs from INT1 (EOC on SOC0).
//
ADC_setupSOC(adcBase, ADC_SOC_NUMBER0, ADC_TRIGGER_EPWM2_SOCA,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER1, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER2, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER3, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER4, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER5, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER6, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER7, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER8, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER9, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER10, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER11, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER12, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER13, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER14, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER15, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
//
// Configure ADCINT1 trigger for SOC1-SOC15
//
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER1,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER2,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER3,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER4,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER5,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER6,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER7,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER8,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER9,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER10,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER11,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER12,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER13,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER14,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER15,
ADC_INT_SOC_TRIGGER_ADCINT1);
//
// Enable ADCINT1 & ADCINT2. Disable ADCINT3 & ADCINT4.
//
ADC_enableInterrupt(adcBase, ADC_INT_NUMBER1);
ADC_enableInterrupt(adcBase, ADC_INT_NUMBER2);
ADC_disableInterrupt(adcBase, ADC_INT_NUMBER3);
ADC_disableInterrupt(adcBase, ADC_INT_NUMBER4);
//
// Enable continuous mode
//
ADC_enableContinuousMode(adcBase, ADC_INT_NUMBER1);
ADC_enableContinuousMode(adcBase, ADC_INT_NUMBER2);
//
// Configure interrupt triggers
//
ADC_setInterruptSource(adcBase, ADC_INT_NUMBER1, ADC_SOC_NUMBER0);
ADC_setInterruptSource(adcBase, ADC_INT_NUMBER2, ADC_SOC_NUMBER15);
}
//
// initializeDMA - Initialize DMA through hard reset
//
void initializeDMA(void)
{
// Perform a hard reset on DMA
DMA_initController();
// Allow DMA to run free on emulation suspend
DMA_setEmulationMode(DMA_EMULATION_FREE_RUN); // DMA_EMULATION_STOP / DMA_EMULATION_FREE_RUN
}
// configureDMAChannels - Initialize DMA ch 1 to transfer ADCA results
void configureDMAChannels(void)
{
// DMA channel 1 set up for ADCA
DMA_configAddresses(DMA_CH1_BASE, (uint16_t *)&adcADataBuffer,
(uint16_t *)ADCARESULT_BASE);
// Perform enough 16-word bursts to fill the results buffer. Data will be
// transferred 32 bits at a time hence the address steps below.
DMA_configBurst(DMA_CH1_BASE, 16, 2, 2);
DMA_configTransfer(DMA_CH1_BASE, (RESULTS_BUFFER_SIZE >> 4), -14, 2);
DMA_configMode(DMA_CH1_BASE, DMA_TRIGGER_ADCA2,
(DMA_CFG_ONESHOT_DISABLE | DMA_CFG_CONTINUOUS_ENABLE |
DMA_CFG_SIZE_32BIT));
DMA_enableTrigger(DMA_CH1_BASE);
DMA_disableOverrunInterrupt(DMA_CH1_BASE);
DMA_setInterruptMode(DMA_CH1_BASE, DMA_INT_AT_END);
DMA_enableInterrupt(DMA_CH1_BASE);
}
Attached is an imgur link to a video of what the graph of the buffer looks like