Part Number: TMS320F28379D
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE
Tool/software:
"Hello, I want the processor to start from the internal flash memory when powered on. I want to load the code while the emulator (JTAG) is connected. Now, in the dual LED application found in C2000ware, I managed to save to FLASH memory using the LAUNCHPAD, both in the application with and without sysconfig. When I cut and restore power to the system, the LEDs continue to light up. However, when I load the same code onto my custom control board, the LEDs do not light up at all. What is the issue here? Can you help me with this?"
in addition, how should I set up these keys required for the boot process I am putting the schematics in my own circuit Oct.

Best Regards,
Enes