This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28P55X: LED cannot blink with LED blink example?

Part Number: LAUNCHXL-F28P55X
Other Parts Discussed in Thread: C2000WARE, SYSCONFIG

Tool/software:

Hi Champs,

I am asking this for our customer.

Use CCS 12.7.1.

Use LED blink example in C2000ware V5.02, with Launchpad FLASH build configuration,

C:\ti\c2000\C2000Ware_5_02_00_00\driverlib\f28p55x\examples\led

After building, flash programming, the user finds the LED is not blinking.

The GPIO used for blinking the LED is tied to GPIO31, which is used on F28P55x control card rather than on P55 LP.

It should use GPIO20, but the the user cannot choose it in the drop-down list.

Would you please help clarify this?

How does the user change the board setting from control card to LP in Sysconfig GUI?

  • Hi Wayne,

    Please select Launchpad option from the SysConfig and rebuild the project.

    The default configuration is meant for control card, you need to switch to Launchpad from SysConfig (open SysConfig -> device view -> switch -> select Launchpad F28p55x in board option.)

    Thanks

    Aswin