This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello to all
I am currently using the MCP2210 SPI module as an SPI Master and the F28335 DSP as an SPI slave. What I want to achieve is that when the MCP2210 sends any SPI data to the DSP, the corresponding GPIO pin is enabled based on the activated bit. (e.g., receiving 0x0001 data -> enabling GPIO0 pin, receiving 0x0002 data -> enabling GPIO1 pin, etc.)
Additionally, and more importantly, I am currently transmitting a total of 16 bits of data, but I want only the 12 bits to activate the GPIO pins according to the activated bits mentioned above. The remaining 4 bits should be used to output the status of which GPIO pins are currently enabled to CCS.
Is it possible to achieve this functionality? If so, I would appreciate any advice on what code needs to be written.
The attached picture shows the current code I am using to activate GPIO pins based on the bits, and another picture shows the received data displayed on CCS when sending SPI data to the DSP via the MCP2210_SPI Terminal program.
Best regards,
Hello,
I cannnot debug/write code for you, but I can offer some suggestions:
If you are transmitting 16 bits of data, the chip select line will need to be low the full time so that the slave/peripheral device is actively receiving the data. You could just send the 16-bit transmissions and then break it up (12-bit and 4-bit) in software after you read it - would that work for your application?
I suppose you could alternatively send the 12 bits of data and other 4 bits in separate transmissions, but given that you need to define your SPI character length (it would have to be at least 12 to accommodate your 12-bit data transmissions), you would have to handle any extra bits (when sending the 4-bit status within a 12-bit transmission) in software after receiving.
Best Regards,
Allison