Part Number: C2000WARE
Tool/software:
Hi team,

Q1: As shown in the above figure, rk -yk is the deviation signal. Why do we need to multiply it by 0.5?

The above figure shows the serial PI in controSUIT. For the deviation signal, it is not multiplied by 0.5
Q2. The output range of NLPID should also be normalized to -1.0~+1.0, right?

According to this, the output unit of ± 1.0 should be adjusted from ÷ 2 to ± 0.5, and then a bias of 0.5 should be added to adjust the controller output to the range of 0 to 1.0, and finally assigned to the duty cycle variable, right?