This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: TMS320F28377S: Safety Measures in a two-channel system

Part Number: TMS320F28377S

Tool/software:

The Safety Concept for the C2000 Industrial Safety package describes in chapter 5,3. the required safety measures based on the FMEA document.

Several Safety Features from the Safety manual are not listed in this chapter.

  1. Is this because some Safety measures can be dispensed with due to the two-channel design?
  2. Are there arguments as to why the requirements could be dispensed with?
  3. Is the FMEA document for this Safety Concept also available?

Dieter