Other Parts Discussed in Thread: SYSCONFIG, C2000WARE, UNIFLASH, LAUNCHXL-F28P65X
Tool/software:
CCS crashes when flashing the f28p659dk-q1 device.
CSS Version: 12.5.0.00007
SysConfig Version: 1.18.0
C2000Ware: 5.1.0.00
Tool: XDS110 Debug Probe
I am trying to flash the f28p659dk-q1 device with production code using the stand-alone XDS110 Debug Probe. However, CSS crashes just after an error below appears;
C28xx_CPU1: Flash Programmer: Missing Flash Programming Settings.
C28xx_CPU1: File Loader: Memory write failed: Unknown error
C28xx_CPU1: GEL: File:C:\....out: Load failed.
I have used UniFlash as an alternative, to erase and flash the f28p659dk-q1 device with the .out file. It flashes successfully but the program is not verified as running correctly.
Note:
The code flashes successfully with CSS on the LaunchXL-F28P65X evaluation board used for development.
And also ledblinky project flashes successfully with the f28p659dk-q1 device.