This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F280039C: LAUNCHXL-F280039C

Part Number: LAUNCHXL-F280039C

Tool/software:

I get a JSON code error when launching debugger for this launchpad ... "launch.json is not a valid JSON file. Expected "," or "}" after property value in JSON at position 380 (lie 14 colum 5)" ....I assume this is the comms file for the USB to PCB protocol ? How can I fix ? Cant find any JSON file source and anyway would have only expected to find object code ? 

I will reload the IDE and examples to see if its a code corruption....report back if that fixes problem....

  • The problem has been isolated with ccmxl editor but this is system stuff and I wont know if "saving" any fix will solve the problem because the TI cloud IDE system will be quarantined no doubt ,,,, I have jpg's but dunno how to transmit them.

    As far as I can tell there is no bracketry asymmetry but my view is very limited.

  • Hi,

    Are you only having this problem with the cloud IDE? If you download CCS do you have the same issue?

    Thanks,

    Ben Collier

  • Yep ... I was resorting to the "fortress desktop" when you answered, but you reinforced my desperation and it all worked as posted. The Thea compiler and IDE looks like it simplifies the initiation to these beautiful devices ? On the old eclipse IDE It seems redundant to select and setup xxml files when the IDE has already autodetected ? Similarly the various demo src for the launchpads Vs the control cards ? I wrote HDK HELP files that DID setup for complex devices (turbines at a power station) and they worked GREAT ...we could simulate failures and all sorts of things for training .....your brilliant products deserve this better and more articulate teaching technology.

    So I could start with Thea ? Seeing it will be the main IDE for most of this project ? Its in late Beta sounds like....

  • Hi,

    So I could start with Thea ?

    Sure, I think you will still need to use ccxml files, but that sounds like a good idea.

    Best Regards,

    Ben Collier