Part Number: TMS320F280039C
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hi
1. In the TRM, I have a question about the boot mode.
In my understanding, for this example:
when the input of GPIO0 and GPIO1 is high, the boot mode is SPI boot(BOOTDEF3),
when the input of GPIO2 is high, the boot mode is flash boot(BOOTDEF4).
The BMSP0-2 equal to the bit0-2, when the input is high, then the bit is 1, otherwise the bit is 0.
Is my understanding correct?

2. If we only need secure boot mode, and the entry address is 0x80000, we can set the configuration as follow:

But what is the function of default mode if I configure as above picture?