Part Number: TMS320F28P550SJ9
Other Parts Discussed in Thread: TMS320F280039C
Tool/software:
Part number for TMS320F28P550SJ9 was not available as option so i have used TMS320F280039C as thread title
this question is for TMS320F28P550SJ9
According to TRM,
Default Boot Modes are done by the default boot mode select pins.
But before checking this GPIO's it reads the OTP_BOOTPIN_CONFIG_KEY
What are the GPIO states before the BOOT mode flow starts ??
If the key is 0x5A it checks BOOTPINCONFIG , BOOTDEF for Custom Boot Modes
My Question is when a fresh out if factory microcontroller is powered ON, all the BOOTPINCONFIG-OTP sections are 0xFFFF and since the GPIO's are floating what will be the CPU default boot mode be ??

If the CPU mode is FLASH, what will be the default FLASH ENTRY POINT (ADDRESS)?
According to datasheet,
But this case the BOOTDEF values are all 0xFFFF??
what will happen in this condition?
this case is for Standalone boot flow (Since no Debugger is connected) and here there is no jump to Wait boot for invalid Boot mode key (as per the Flow diagram in TRM).