Tool/software:
Hi,
I have tried working with TMS320F28388D as EtherCAT slave and TwinCAT in PC as EtherCAT master. I would like to know if two TMS320F28388D based controller cards can be used to perform an EtherCAT master slave communication? If yes, are there any resources detailing the possibility of using the same device as an EtherCAT master? Is the EtherCAT master stack code available?