Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hi team ,
We are working on F28379D Launch pad , We need to run FLASH api through RAM could you please help us .
We Tried in below method :
main.c
extern uint16_t Flash_API_LoadStart;
extern uint16_t Flash_API_LoadEnd;
extern uint16_t Flash_API_RunStart;
extern uint16_t Flash_API_LoadSize;
void CopyFlashAPIToRAM(void)
{
uint16_t *loadAddr = (uint16_t *)&Flash_API_LoadStart;
uint16_t *runAddr = (uint16_t *)&Flash_API_RunStart;
uint16_t loadSize = (uint32_t)&Flash_API_LoadEnd - (uint32_t)&Flash_API_LoadStart;
memcpy(runAddr, loadAddr, loadSize);
}
void load(char *load,char *start, uint16_t size)
{ do
{
*start = *load;
start++;
load++;
} while (--size);
}
load((char *)&Flash_API_LoadStart,
(char *)&Flash_API_RunStart,
(uint16_t)&Flash_API_LoadSize);
.cmd file:
FlashAPIcode : LOAD = FLASHD,
RUN = RAMGS14,
LOAD_START(Flash_API_LoadStart),
LOAD_END(Flash_API_LoadEnd),
LOAD_SIZE(Flash_API_LoadSize),
RUN_START(Flash_API_RunStart),
RUN_END(FlashApi_RunEnd),
RUN_SIZE(FlashApi_RunSize),
PAGE = 0, ALIGN(8)
Kindly Suggest the correction or steps to do that.
Thanks and Regards
Madan Mohan N