This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28386D: using uniflash to write specific security registers and settings

Part Number: TMS320F28386D
Other Parts Discussed in Thread: UNIFLASH

Tool/software:

Hi,

a customer is having trouble getting Uniflash to work at setting registers to configure the device's security settings and this is blocking current development. 

We are trying to do something simple right now (shown on the screenshots below). Setting Z1-GPREG3 to 0xFFFFFF03 should simply define that flash boot from 0x8'0000 is the only defined boot method (boot mode 0).

Clicking on the "Program" button right below the Z1-GPREGX section raises the error at the bottom of the screen (Please make sure the memory location you are programming have not already been programmed.) As per the memory browser, the 0x7'8008 (and subsequent) locations are all untouched.

We are able to do things like flash the device with a binary and erase the flash so we doubt that this is a connection or setup issue. The work is on Linux but also tried on Windows with the same results.

Is there some documentation available that would help me understand what I'm not doing correctly here? 

Regards,

--Gunter