Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hi everyone,
I am currently working on the following tasks and would appreciate your guidance:
I have three sets of voltage and current data obtained from power system simulation software. These signals were sampled at 10 kHz for a 60 Hz system, resulting in approximately 52,000 points for each signal. The data have been processed to range between 0 and 4095. My goal is to store this data in flash memory, allowing it to be read and transferred in real-time to an MCU for operations such as filtering, downsampling, FFT computation, and protection decisions.
After exploring some discussions on this forum, I learned that the Flash API might be suitable for writing data to flash memory for later use during real-time operations. However, as I am new to this topic, I am encountering challenges. Specifically, I understand that the data must first be programmed into memory, but I have been unable to get the flash programming example in Code Composer Studio (CCS) to work.
Here are my questions:
- Is it feasible to achieve the workflow I’ve described?
- Does my proposed process make sense, or are there any steps I am missing?
- Are there any beginner-friendly guides or resources for using the Flash API?
Thank you in advance for your support.
Best regards,