Other Parts Discussed in Thread: UNIFLASH
Tool/software:
Hello,
I am currently running into this error when trying to flash my TMS320F280039C using Simulink integrated with Code Composer Studio 12.8.1:
Error connecting to the target: (Error -1135 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 20.0.0.3298)
I successfully flashed my TMS320F280039C twice before using the same code, and this error occurred the third time with the same code. I have tried running a simple code in CCS, but debug came back with the same error. The "Test Connection" comes out successful. I have tried updating my CCS and using the UNIFLASH tool, which still runs into the same error when trying to connect. LEDs 1:A, 3:A, and D3 all light up RED, BLUE, and GREEN respectively, and LED 2:A weakly flashes BLUE once when trying to connect. I have also checked if the java based jar files are present in the class path, and they are.
I am not sure how to proceed, or even how to determine if the on-board XDS110 debugger is broken. I would appreciate the help.