This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C: What happens if DAC ramps down to zero?

Part Number: TMS320F280039C

Tool/software:

Hi champs,

I am asking this for our customer.

From TRM spruiw9c (https://www.ti.com/lit/pdf/spruiw9), see below red box.

The user uses DACH ramp generator to trip a EPWM to low.

When the DACH ramps down to zero and if CMPINxP is a little bit lower than 0x0 because of minus comparator input offset, which means there is likely no COMPHSTS=1,

1) Will the DACH still be recharged to RAMPMAXREFS "right after" it becomes 0x0? Or the DACH will not be recharged until EPWMSYNCPER (at EPWM counter=0)?

2) What happens when there is no COMPHSTS=1? Does that mean the PWM output can be 100% duty because there is no trip event?