This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I am walking through the lab and when I'm trying to run the SFRA, I keep getting the following error:
What could be causing this?
I'm using CCS Theia
Hi Ki,
I'm using the Digital Power SDK Version 5.04.00.00 and the TIDM-DC-DC-BUCK reference design. Trying to follow along in the user guide's labs.
I'm using CCS Theia version 1.5.1.00003.
Sysconfig version 1.22.0
I see you have two versions detected. When you build your project, which one is used? You can tell by looking at the build output:
Thanks. Are you doing any specific action in the IDE to trigger the error? I have been playing around with the project but have not triggered the error yet.
Thanks.
ki
I don't think so. I tried uninstalling and reinstalling code composer altogether and I was still getting the same error when trying to open the SFRA.
You mentioned you were following a lab. Is it the lab in this document: https://dev.ti.com/tirex/explore/node?node=A__AMJRCjyqPWotKFi5OZWM7A__digital_power_c2000ware_sdk_software_package__5C6SEVO__LATEST ?
Thank you. I can reproduce this. I also tried with the latest CCS 20.0.2 with sysconfig 1.22 but I had the same issue. We are investigating. Thank you.
Engineering is investigating. It looks like a bug with CCS Theia/20. CCS 12.x does not have this issue.
Thank you for the update. Looking forward to what you discover.
Could this effect me running the SFRA tool with code that I generate in CCS Theia?
It appears that the button simply executes the SFRA_GUI.exe in <C2000Ware DigitalPower SDK INSTALL DIR>\powerSUITE\source\utils with a parameter of the directory of the project.
So is CCS having trouble finding it?
I don't have all the details but CCS relies on an API to find the application and it looks like that API is not working correctly in CCS Theia/20 (it works in CCS 12.x).