This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
#include "f28x_project.h" #include "sysctl.h" //#include "f2838x_epwm.h" // DEFINIZIONI #define MYPWM_FREQUENCY 40000 #define MYDEADBAND_VALUE 0.001 #define OSC_FREQ 25000000 uint32_t MYSYSCLK; uint32_t tbprd; uint32_t clockDivider; uint32_t timebaseclk; //PROTOTIPI void inizializzapwm1(void); void inizializzapwm2(void); // Main void main(void) { // Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks //This example function is found in the f2838x_sysctrl.c file. InitSysCtrl(); // enable PWM1, PWM2 CpuSysRegs.PCLKCR2.bit.EPWM1=1; CpuSysRegs.PCLKCR2.bit.EPWM2=1; // For this case just init GPIO pins for ePWM1, ePWM2, ePWM3 // These functions are in the f2838x_epwm.c file InitEPwm1Gpio(); InitEPwm2Gpio(); // // Step 3. Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts // DINT; // // Initialize the PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the f2838x_piectrl.c file. // InitPieCtrl(); // // Disable CPU interrupts and clear all CPU interrupt flags: // IER = 0x0000; IFR = 0x0000; // // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in f2838x_defaultisr.c. // This function is found in f2838x_pievect.c. // EALLOW; CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 0; EDIS; inizializzapwm1(); EALLOW; CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1; EDIS; for(;;) { asm (" NOP"); } } void inizializzapwm1() { // // Setup TBCLK //ClkCfgRegs.PERCLKDIVSEL.bit.EPWMCLKDIV = 0x1; MYSYSCLK = SysCtl_getClock(OSC_FREQ); EPwm1Regs.TBCTL.bit.HSPCLKDIV = 2; // Clock ratio to SYSCLKOUT EPwm1Regs.TBCTL.bit.CLKDIV = 2; clockDivider = EPwm1Regs.TBCTL.bit.HSPCLKDIV * EPwm1Regs.TBCTL.bit.CLKDIV; tbprd = (MYSYSCLK/clockDivider)/(2*MYPWM_FREQUENCY); EPwm1Regs.TBPRD = tbprd; EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; // Load registers every ZERO EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW; EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; EPwm1Regs.CMPA.bit.CMPA = tbprd/2; // Set compare A value duty 50% EPwm1Regs.CMPB.bit.CMPB = tbprd/2; // Set Compare B value duty 50% EPwm1Regs.AQCTLA.bit.CAU = AQ_SET; // Set PWM1A on event A, up count EPwm1Regs.AQCTLA.bit.CAD = AQ_CLEAR; // Clear PWM1A on event A, down count EPwm1Regs.AQCTLB.bit.CBU = AQ_CLEAR; // Set PWM1B on event B, up count EPwm1Regs.AQCTLB.bit.CBD = AQ_SET; // Clear PWM1B on event B, down count EPwm1Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; EPwm1Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC; EPwm1Regs.DBCTL.bit.IN_MODE = DBA_ALL; EPwm1Regs.DBRED.bit.DBRED = 20; EPwm1Regs.DBFED.bit.DBFED = 20; }
Dear Texas support,
I am a PhD student at ENEA in Italy, and I would like to create a code that automatically updates the Time Base Period (TBPRD) value to achieve the desired PWM signal frequency for a given frequency. In my code, the Time Base Period changes, but it does not allow me to achieve the desired PWM frequency. I would greatly appreciate your help in understanding where I might be going wrong.
Thank you in advance for your assistance.
Hello Gianluca,
Please find the app note C2000 ePWM Developer’s Guide which simplifies configuration including calculating TBPRD. What you have calculated is for up or down counter. Please use up-down counter formulae to get correct value.
Also, you can refer/use our ePWM examples in C2000Ware (C:\ti\c2000\C2000Ware_5_02_00_00\examples). You can download and install the same from https://www.ti.com/tool/C2000WARE. These example also contains Ti SysConfig tool that will make configurating ePWM peripheral easier.
Regards,
Sumit