Part Number: TMS320F28P650DK
Tool/software:
Hi TI experts,
I'm working on "tida_010936_ganhfmd" project. it was working fine. now I want to run the entire motor control ISR from CLA and all the variables, structures were extended to CLA. I'm facing problems with CLAcos and CLAsin functions. from CLA Math Library User's Guide section 4, I've added cla1_math_library_fpu32_eabi and included it linker search path. code is built but when im running the code there is no output.

I'm able to see the CLAcos and CLAsin tables in .map file

what should be the way forward?
Thanks & Regards
Raghu