Part Number: TMS320F280039C
Other Parts Discussed in Thread: PMP41006,
Tool/software:
Hello,
We are in the process of developing a PFC + LLC system.
In PMP41006, the controllers are separately prepared for PFC and LLC. Is it possible to integrate the PFC and LLC controllers into one?
The TMS320F280039C appears to have a CPU capacity of 120 MIPS + CLA 120 MIPS, totaling 240 MIPS.
Our PFC is planned to be of the T-type. In your TIDA01606.2, the CPU load for the T-type PFC is estimated to be 54 MIPS. I couldn't find an example of the CPU load for LLC, but if the load is similar, I thought that it might be feasible to integrate the controllers into one. Is that possible?

Even if there are enough MIPS, is there a possibility of compromising real-time performance? If real-time performance is critical, can it be improved by choosing a higher-level MPU?"
Of course, since the controller block is isolated from the main circuit block, I believe there shouldn't be any electrical issues with using one controller for both PFC and LLC.
Best Regards,
YUKIOOYAMA