This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28027F: TMS320F28027 with DRV8301 to run bldc motor

Part Number: TMS320F28027F
Other Parts Discussed in Thread: MOTORWARE

Tool/software:

Hi

I am using Project Lab 11 in MotorWare, and I'm encountering some errors in the f28027.cmd file. Could someone please provide some assistance?

Description	Resource	Path	Location	Type
#10010 errors encountered during linking; "proj_lab11.out" not built	proj_lab11		 	C/C++ Problem
#10099-D program will not fit into available	F28027.cmd	/proj_lab11	line 135	C/C++ Problem
gmake: *** [proj_lab11.out] Error 1	proj_lab11		 	C/C++ Problem
gmake: Target 'all' not remade because of errors.	proj_lab11		 	C/C++ Problem
#10247-D creating output section ".cio" without a SECTIONS	proj_lab11		 	C/C++ Problem