Tool/software:
Hello, i am a new to study LAUNCHXL-F280049C board. i have the question so bellow:
1. Connecting the board with PC, then open the CCS, but the CCS can not detect the board. and the same time, the LED2 on the board is off, LED3 is ON.
Hi Wu,
The LED looks correct, one will indicated that debugger is operational and the other will indicate data transmission between the C2000 microcontroller and the PC.
What do you mean the CCS is not detecting the board? You can double check by testing the led_blinky example from our C2000Ware SDK example
Regards,
Peter